Regarding the display used on the SABRE-SD board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Regarding the display used on the SABRE-SD board

Jump to solution
764 Views
patcharasirigul
Contributor II

Hello everyone,

We're planning to use display for connecting with SABRE board, but we're looking for another display to use with it. The type of interface we use is LVDS. I've read the datasheet of display the SABRE board used is : http://boundarydevices.com/wp-content/uploads/2013/06/HSD100PXN1-A00-C11-1.0.pdf

I found the pin assignment on page 13. The pin 4, pin 6 and pin 7 are V_EDID, CLK_EDID and DATA_EDID. but the display we are planning to use, it does't have these pin.

I'd like to know what the pin 4, 6 and 7 is.

Can I connect the another display without pin 4, 6 and 7 ?

and What is the effect if I connect the display without these pin ?

Please help me.

Thank you so much.

Labels (3)
0 Kudos
Reply
1 Solution
699 Views
igorpadykov
NXP Employee
NXP Employee

Hi Patchara

this particular HannStar lvds LCD has i2c ID data for identification

(similar to hdmi monitors). Not all lvds LCDs has such ID signals and it is

not used in BSP. You can any use suitable lvds LCD without these signals.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
700 Views
igorpadykov
NXP Employee
NXP Employee

Hi Patchara

this particular HannStar lvds LCD has i2c ID data for identification

(similar to hdmi monitors). Not all lvds LCDs has such ID signals and it is

not used in BSP. You can any use suitable lvds LCD without these signals.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply