Hi all, I'm using kernel 4.1 from yocto krogoth on an IMX6q board.
When i ask for the reboot, the board is not rebooted. After invastigation it appears that restart function in the DT_MACHINE_START have been suppressed, so there is no more restart function.
Can anyone tell me how IMX6q boards can still be resetted ?
Why was this function suppressed in last kernel ?
Thanks by advance.
Regards.
Christian
Hi Christian!
Did you resolve this issue? I have the same problem with a 4.9.11 kernel. I've added the 'mxc_restart' method to the DT_MACHINE_START table but reboot is still not working... Did you get it working?
Thanks!
Jorge
Hello,
please use NXP Linux. Linux command "reboot" works.
Also, You may apply "shutdown -r 0".
Summary Page :
i.MX 6 Series Software and Development Tool|NXP
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------