Questions about DMA mode for iMX28 auart

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Questions about DMA mode for iMX28 auart

1,023件の閲覧回数
lategoodbye
Senior Contributor I

Hi,

 

i'm a application developer and have some questions about the mxs-auart under Linux 2.6.35 (Freescale BSP) and the iMX28 platform:

 

Where do i get the information at runtime, which mode (DMA on/off) the auart is running?

Can i enable or disable DMA mode at runtime for the auart?

Are there any disadvantages using DMA mode for mxs-auart?

Does the DMA mode support marking of parity and framing errors?

Is there more documentation about auart than in the reference manual for the EVK?

Thanks in advance

ラベル(1)
0 件の賞賛
返信
1 返信

667件の閲覧回数
colinmoloney
Contributor II

Yes.  I'd like to know the same answers, especially for the more recent device-tree builds (eg morty or rocko)

0 件の賞賛
返信