Hi team,
I would like to ask about the bandgap reference voltage calibration.
i.MX28 reference manual(MCIMX28RM Rev.2) says as below.(Table 38-1)
"But if the bandgap reference is calibrated using the fuses, then …"
Could you show me what the 'calibration with fuses' is?
And could you show me the procedure of the calibrate with fuses?
Thanks,
Miyamoto
解決済! 解決策の投稿を見る。
Hi AVNET JAPAN FAE
ADC 'calibration with fuses' is not supported
(not tested/no example codes).
Also bandgap voltage doesn't output to pad and
can't be monitored on pad, so it is difficult to calibrate bandgap voltage for i.MX28.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi AVNET JAPAN FAE
ADC 'calibration with fuses' is not supported
(not tested/no example codes).
Also bandgap voltage doesn't output to pad and
can't be monitored on pad, so it is difficult to calibrate bandgap voltage for i.MX28.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Chipexpert,
Can I understand as below?
The internal bandgap reference voltage is connected to LRADC channel-14 internally, but user cannot monitor it.
Then the bandgap reference voltage cannot be calibrated.
BR,
Miyamoto
Hi Miyamoto
yes this is correct.
Best regards
chip