Question, i.MX28 DISABLE_STEPPING bit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX28 DISABLE_STEPPING bit

1,102件の閲覧回数
Aemj
Contributor IV

Dear team,

I would like to ask about the DISABLE_STEPPING bit in HW_POWER_VDDDCTRL register of i.MX28.

(1)

If one desires to disable default stepping behavior, does one need to set DISABLE_STEPPING-bit every time TRG bit is changed?

(2)

And please let me know the correct sequence on setting DISABLE_STEPPING bit.

Change TRG then set DISABLE_STEPPING bit, Or, set DISABLE_STEPPING then change TRG?

(3)

Is it possible for internal DCDC converter to have incorrect voltage by incorrect procedure of setting DISABLE_STEPPING bit?

Thanks,

Miyamoto

ラベル(1)
0 件の賞賛
返信
1 返信

1,032件の閲覧回数
art
NXP Employee
NXP Employee

Q1. If one desires to disable default stepping behavior, does one need to set DISABLE_STEPPING-bit every time TRG bit is changed?

A1. No.

Q2. Change TRG then set DISABLE_STEPPING bit, Or, set DISABLE_STEPPING then change TRG?

A2. Set DISABLE_STEPPING then change TRG.

Q3. Is it possible for internal DCDC converter to have incorrect voltage by incorrect procedure of setting DISABLE_STEPPING bit?

A3. This is not a known issue.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信