i.mx28使用SGTL5000录音噪声问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.mx28使用SGTL5000录音噪声问题

Jump to solution
914 Views
阳黄
Contributor I

控制芯片是i.mx283,系统是wince6.0,用的官方的BSP,录音和放音部分电路和官方一样。现在放音正常,录音只能听见一点点录进去的声音,噪声很大,录音使用的是mic,LOOPBACK模式没有什么噪声,DUPLEX模式噪音很大。请问可能是什么问题,谢谢。

Labels (2)
1 Solution
667 Views
阳黄
Contributor I

好的,谢谢,问题解决了,是SAIF1模块初始化位置不正确导致的,需要把官方BSP中SAIF1模块的初始化位置下移就可以了。

View solution in original post

2 Replies
667 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi 阳,

You can refer to Re: SGTL5000 CODEC line-in noise on i.MX28 thread, hope this can help you.
Have a great day,
Dan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

668 Views
阳黄
Contributor I

好的,谢谢,问题解决了,是SAIF1模块初始化位置不正确导致的,需要把官方BSP中SAIF1模块的初始化位置下移就可以了。