Question about yocto, imx28evk, MfgTool and NAND

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about yocto, imx28evk, MfgTool and NAND

ソリューションへジャンプ
8,601件の閲覧回数
persmitt
Contributor III

Hi

I am having trouble with the spam filter so I will split this question into several replies on the same thread to figure out why the spam filter hates me ;-)

I am getting started with an embedded Linux project using Yocto and the i.MX28 evk. So far things have gone pretty well but I have run into a hurdle when trying to get Linux to boot from the NAND flash instead of the SD card.

Before I go more into the questions I will just summarize quickly of what I have done to get a general idea of where I stand.

For starters I followed Yocto Training - HOME to get started with the Yocto concept. I took the generated image, dd it to an SD card and then started Linux on the eval board without any problems. I also played around by adding an ftp-server, sshd and apache just to learn a bit more how to add packages.

 

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 解決策
5,054件の閲覧回数
persmitt
Contributor III

After my latest post I had a u-boot and a kernel flashed to NAND. I was however mistaken about the load address. Fortunately someone with more knowledge had prepared U-boot with default parameters.

=> printenv loadaddr

loadaddr=0x42000000

I have no clue why it is at 0x42000000 and not at 0x40008000 that I got from uboot-mkimage but the U-boot preloaded value was correct in my case. Anyone with input on this would be appreciated.

Once the kernel has the correct load address it will get much further during startup, all the way to mounting the root file system. For the file system it seemed that ubifs was the modern way to go so thats what I did.

Flashing a ubifs file system on a nand can be done in two ways. You can, for one, flash it with a generic NAND flasher. This requires a ubi image which is created by running ubinize on an existing ubifs image.

The other alternative is to flash a ubifs image through U-Boot, which is what I decided to do. The ubifs image is created by running mkubifs but this is handled automatically by bitbake if you have set ubifs as a target in conf/machine/imx28evk.conf.

IMAGE_FSTYPES ?= "tar.bz2 ext3 uboot.mxsboot-sdcard sdcard ubifs"

However building the ubifs image requires certain parameters set in the same file (conf/machine/imx28evk.conf)

MKUBIFS_ARGS = "--min-io-size 2048 --leb-size 126976 --max-leb-cnt 864"

These values can be found by running ubiattach -m 1 /dev/ubi_ctrl (requires packages mtd-utils and mtd-utils-ubifs) in Linux on your target system. The easiest way to do this is to boot on an SD card, see Task #4 - Deploy and test

However depending on your bootargs you might not have access to /dev/mtdX. If the mtd device is missing, reboot and enter U-Boot and add gpmi (Can not see the NAND device /dev/mtd0 or /dev/mtd1 for micron MT29F1G08ABADA) to the mmcargs.

setenv mmcargs setenv bootargs gpmi ${mtdparts} console=${console_mainline},${baudrate} root=${mmcroot}

run mmcboot

Your /dev/mtdX should be available now. The NAND partitions does not work like normal file system partitions, instead they are entirely logical and setup with an address and a size. In U-Boot the NAND partitions can be setup neatly with the command mtdparts and for many imx boards that can translate just nicely to a booted Linux, but not the imx28. The other boards have an external file where the NAND partitions can be configured but the imx28 has the partition hardcoded in the driver. It can be found (grep for mtd_partition) and modified but then it must be maintained as a kernel patch every time there is an upgrade. Instead I opted for going with the default partition the imx28 nand driver offers: /dev/mtd0 20MiB, /dev/mtd1 has the rest. Verify the numbers using mtdinfo command. My strategy is to put bootloader, environment and kernel in /dev/mtd0 and in /dev/mtd1 I put filesystems by using multiple ubifs volumes in the same partition.

So analyzing the output from ubiattach -m 1 /dev/ubi_ctrl

UBI: attaching mtd1 to ubi0

UBI: physical eraseblock size:   131072 bytes (128 KiB)

UBI: logical eraseblock size:    126976 bytes

UBI: smallest flash I/O unit:    2048

UBI: VID header offset:          2048 (aligned 2048)

UBI: data offset:                4096

UBI: attached mtd1 to ubi0

UBI: MTD device name:            "gpmi-nfc-general-use"

UBI: MTD device size:            108 MiB

UBI: number of good PEBs:        864

UBI: number of bad PEBs:         0

UBI: max. allowed volumes:       128

UBI: wear-leveling threshold:    4096

UBI: number of internal volumes: 1

UBI: number of user volumes:     0

UBI: available PEBs:             852

UBI: total number of reserved PEBs: 12

UBI: number of PEBs reserved for bad PEB handling: 8

UBI: max/mean erase counter: 1/1

UBI: image sequence number: 0

UBI: background thread "ubi_bgt0d" started, PID 397

UBI device number 0, total 864 LEBs (109707264 bytes, 104.6 MiB), available 852 LEBs (108183552 bytes, 103.2 MiB), LEB size 126976 by)

Use the values to set the MKUBIFS_ARGS to get a ubifs image that will work for your NAND flash.

Now since we are reconsidering the partitioning lets recap where to put stuff and start from the point where we only have u-boot on the nand.

First lets build the partition table using mtdparts default and then we delete the incorrectly placed file system.

mtdparts default

mtdparts del filesystem

Then we place the file system after the first 20MiB. I use a 128MiB NAND here.

mtdparts add nand0 0x06C00000@0x1400000 filesystem

The partition table should look like this now

=> mtdparts

device nand0 <gpmi-nand>, # parts = 7

#: name                size            offset          mask_flags

0: bootloader          0x00300000      0x00000000      1

1: environment         0x00080000      0x00300000      0

2: redundant-environment0x00080000     0x00380000      0

3: kernel              0x00400000      0x00400000      0

4: fdt                 0x00080000      0x00800000      0

5: ramdisk             0x00800000      0x00880000      0

6: filesystem          0x06c00000      0x01400000      0

Lets save the partition table to the environment.

saveenv

Now let us first flash the kernel where it is supposed to be. As usual we download it from a USB thumb since I haven't gotten to setup TFTP yet.

usb start

fatls usb 0:1

nand erase.part kernel

fatload usb 0:1 ${loadaddr} uimage-imx28evk.bin

nand write ${loadaddr} kernel

Now the kernel is in place, lets setup the kernel boot arguments. U-boot comes with a default environment nandargs which is almost entirely correct for us.

nandargs=setenv bootargs console=${console_mainline},${baudrate} rootfstype=ubifs ubi.mtd=6 root=ubi0_0 ${mtdparts}

The part that is incorrect for us is ubi.mtd=6 as we are planning to have the filesystem on mtd1. So we take the setenv part and runs it manually. It is also important to add the gpmi argument so the nand driver will load.

setenv bootargs gpmi console=${console_mainline},${baudrate} rootfstype=ubifs ubi.mtd=1 root=ubi0_0 ${mtdparts}

setenv bootcmd 'nboot kernel; bootm'

saveenv

We can now try to boot and should get as far as trying to mount the root file system.

So now it is time to put in our ubifs image into nand. First we load the ubifs image into memory.

usb start

fatls usb 0:1

fatload usb 0:1 ${loadaddr} core-image-minimal-imx28evk.ubifs

Then we erase the filesystem partition.

nand erase.part filesystem

We set the ubi subsystem to work with the filesystem partition

ubi part filesystem

We create a volume. Since we don't set type or size it becomes dynamic and covers the entire size.

ubi create rootfs

Write the loaded image to the newly created volume. If we had created multiple volumes we chose which volume to receive the image. Useful for having multiple filesystems/partitions.

ubi write ${loadaddr} rootfs ${filesize}

Finally we mount the file system locally to verify that it looks ok.

ubifsmount ubi0:rootfs

ubifsls

Now we can reboot and this time Linux should start properly. It did for me and I hope it will work for you too!

元の投稿で解決策を見る

0 件の賞賛
返信
13 返答(返信)
5,054件の閲覧回数
sonuabraham
Contributor I

Hi Per Smitt,

Can you let us know how the following crash in the rootfs was solved . I am getting similar error when trying to boot an Angstrong image on imx28evk board.

 

undefined instruction

pc : [<40008010>]          lr : [<47f38440>]

sp : 47b32d70  ip : 00000000     fp : 00000000

r10: 00000000  r9 : 47b32f38     r8 : 47b417dc

r7 : 00000000  r6 : 40008000     r5 : 47f9f724  r4 : 00000000

r3 : 47b32fe0  r2 : 40000100     r1 : 000009e3  r0 : 47b32fe0

Flags: nZCv  IRQs off  FIQs off  Mode SVC_32

Resetting CPU ...

Thanks in advance,

Sonu Abraham

0 件の賞賛
返信
5,054件の閲覧回数
lzh_kc
Contributor I

Hi persmitt

You said you had  "played around by adding an ftp-server, sshd and apache just to learn a bit more how to add packages",

I'm now trying to add apcahe,mysql and php into my image, but don't know how.

Here are what i have tryed:

I do bitbake php first, and then add "php" and "php-cli" (which inspired by an answer in question Re: Adding php package to fsl-image-machine-test )  into the CORE_IMAGE_EXTRA_INSTALL varible in local.conf, then do "bitbake fsl-image-qt5". I run the image on my imx6 board and happiely find that php works fine.

But when i want to add apache and mysql, that's not work, I find a .bb file for apache: "source/meta-openembedded/meta-webserver/recipes-httpd/apache2/apache2_2.4.10.bb", but I don't know how to use it.

As to mysql, I do as adding php, and I get only a .so file in a deep chlid tree in /usr/lib on the imx6 board.

So how do I get wrong , how do you add apache? Please help me, many thanks!

@persmitt

0 件の賞賛
返信
5,054件の閲覧回数
persmitt
Contributor III

Just add apache2 to the same variable. If you find a recipe (in this case apache2_2.4.10.bb) simply truncate the name at the underscore and add it to your CORE_IMAGE_EXTRA_INSTALL. That should add apache to your build.

0 件の賞賛
返信
5,055件の閲覧回数
persmitt
Contributor III

After my latest post I had a u-boot and a kernel flashed to NAND. I was however mistaken about the load address. Fortunately someone with more knowledge had prepared U-boot with default parameters.

=> printenv loadaddr

loadaddr=0x42000000

I have no clue why it is at 0x42000000 and not at 0x40008000 that I got from uboot-mkimage but the U-boot preloaded value was correct in my case. Anyone with input on this would be appreciated.

Once the kernel has the correct load address it will get much further during startup, all the way to mounting the root file system. For the file system it seemed that ubifs was the modern way to go so thats what I did.

Flashing a ubifs file system on a nand can be done in two ways. You can, for one, flash it with a generic NAND flasher. This requires a ubi image which is created by running ubinize on an existing ubifs image.

The other alternative is to flash a ubifs image through U-Boot, which is what I decided to do. The ubifs image is created by running mkubifs but this is handled automatically by bitbake if you have set ubifs as a target in conf/machine/imx28evk.conf.

IMAGE_FSTYPES ?= "tar.bz2 ext3 uboot.mxsboot-sdcard sdcard ubifs"

However building the ubifs image requires certain parameters set in the same file (conf/machine/imx28evk.conf)

MKUBIFS_ARGS = "--min-io-size 2048 --leb-size 126976 --max-leb-cnt 864"

These values can be found by running ubiattach -m 1 /dev/ubi_ctrl (requires packages mtd-utils and mtd-utils-ubifs) in Linux on your target system. The easiest way to do this is to boot on an SD card, see Task #4 - Deploy and test

However depending on your bootargs you might not have access to /dev/mtdX. If the mtd device is missing, reboot and enter U-Boot and add gpmi (Can not see the NAND device /dev/mtd0 or /dev/mtd1 for micron MT29F1G08ABADA) to the mmcargs.

setenv mmcargs setenv bootargs gpmi ${mtdparts} console=${console_mainline},${baudrate} root=${mmcroot}

run mmcboot

Your /dev/mtdX should be available now. The NAND partitions does not work like normal file system partitions, instead they are entirely logical and setup with an address and a size. In U-Boot the NAND partitions can be setup neatly with the command mtdparts and for many imx boards that can translate just nicely to a booted Linux, but not the imx28. The other boards have an external file where the NAND partitions can be configured but the imx28 has the partition hardcoded in the driver. It can be found (grep for mtd_partition) and modified but then it must be maintained as a kernel patch every time there is an upgrade. Instead I opted for going with the default partition the imx28 nand driver offers: /dev/mtd0 20MiB, /dev/mtd1 has the rest. Verify the numbers using mtdinfo command. My strategy is to put bootloader, environment and kernel in /dev/mtd0 and in /dev/mtd1 I put filesystems by using multiple ubifs volumes in the same partition.

So analyzing the output from ubiattach -m 1 /dev/ubi_ctrl

UBI: attaching mtd1 to ubi0

UBI: physical eraseblock size:   131072 bytes (128 KiB)

UBI: logical eraseblock size:    126976 bytes

UBI: smallest flash I/O unit:    2048

UBI: VID header offset:          2048 (aligned 2048)

UBI: data offset:                4096

UBI: attached mtd1 to ubi0

UBI: MTD device name:            "gpmi-nfc-general-use"

UBI: MTD device size:            108 MiB

UBI: number of good PEBs:        864

UBI: number of bad PEBs:         0

UBI: max. allowed volumes:       128

UBI: wear-leveling threshold:    4096

UBI: number of internal volumes: 1

UBI: number of user volumes:     0

UBI: available PEBs:             852

UBI: total number of reserved PEBs: 12

UBI: number of PEBs reserved for bad PEB handling: 8

UBI: max/mean erase counter: 1/1

UBI: image sequence number: 0

UBI: background thread "ubi_bgt0d" started, PID 397

UBI device number 0, total 864 LEBs (109707264 bytes, 104.6 MiB), available 852 LEBs (108183552 bytes, 103.2 MiB), LEB size 126976 by)

Use the values to set the MKUBIFS_ARGS to get a ubifs image that will work for your NAND flash.

Now since we are reconsidering the partitioning lets recap where to put stuff and start from the point where we only have u-boot on the nand.

First lets build the partition table using mtdparts default and then we delete the incorrectly placed file system.

mtdparts default

mtdparts del filesystem

Then we place the file system after the first 20MiB. I use a 128MiB NAND here.

mtdparts add nand0 0x06C00000@0x1400000 filesystem

The partition table should look like this now

=> mtdparts

device nand0 <gpmi-nand>, # parts = 7

#: name                size            offset          mask_flags

0: bootloader          0x00300000      0x00000000      1

1: environment         0x00080000      0x00300000      0

2: redundant-environment0x00080000     0x00380000      0

3: kernel              0x00400000      0x00400000      0

4: fdt                 0x00080000      0x00800000      0

5: ramdisk             0x00800000      0x00880000      0

6: filesystem          0x06c00000      0x01400000      0

Lets save the partition table to the environment.

saveenv

Now let us first flash the kernel where it is supposed to be. As usual we download it from a USB thumb since I haven't gotten to setup TFTP yet.

usb start

fatls usb 0:1

nand erase.part kernel

fatload usb 0:1 ${loadaddr} uimage-imx28evk.bin

nand write ${loadaddr} kernel

Now the kernel is in place, lets setup the kernel boot arguments. U-boot comes with a default environment nandargs which is almost entirely correct for us.

nandargs=setenv bootargs console=${console_mainline},${baudrate} rootfstype=ubifs ubi.mtd=6 root=ubi0_0 ${mtdparts}

The part that is incorrect for us is ubi.mtd=6 as we are planning to have the filesystem on mtd1. So we take the setenv part and runs it manually. It is also important to add the gpmi argument so the nand driver will load.

setenv bootargs gpmi console=${console_mainline},${baudrate} rootfstype=ubifs ubi.mtd=1 root=ubi0_0 ${mtdparts}

setenv bootcmd 'nboot kernel; bootm'

saveenv

We can now try to boot and should get as far as trying to mount the root file system.

So now it is time to put in our ubifs image into nand. First we load the ubifs image into memory.

usb start

fatls usb 0:1

fatload usb 0:1 ${loadaddr} core-image-minimal-imx28evk.ubifs

Then we erase the filesystem partition.

nand erase.part filesystem

We set the ubi subsystem to work with the filesystem partition

ubi part filesystem

We create a volume. Since we don't set type or size it becomes dynamic and covers the entire size.

ubi create rootfs

Write the loaded image to the newly created volume. If we had created multiple volumes we chose which volume to receive the image. Useful for having multiple filesystems/partitions.

ubi write ${loadaddr} rootfs ${filesize}

Finally we mount the file system locally to verify that it looks ok.

ubifsmount ubi0:rootfs

ubifsls

Now we can reboot and this time Linux should start properly. It did for me and I hope it will work for you too!

0 件の賞賛
返信
5,054件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Try posting this question to the meta-fsl-arm mailing list.

0 件の賞賛
返信
5,054件の閲覧回数
persmitt
Contributor III

A good idea but I actually managed to solve pretty much everything so I will post a detailed description of what I did and which pitfalls I fell in so hopefully others can find all the information in one place. It took some 8-10 hours of googling but step by step all question marks were solved. :smileyhappy:

0 件の賞賛
返信
5,053件の閲覧回数
persmitt
Contributor III

I have gotten a bit further now in my digging to run an i.MX28 from NAND. After investigating MfgTool for a bit I came to the conclusion that it wanted sb files. I modified my machine config to output sb files.

diff --git a/conf/machine/imx28evk.conf b/conf/machine/imx28evk.conf

index d4f1ad6..2b6939e 100644

--- a/conf/machine/imx28evk.conf

+++ b/conf/machine/imx28evk.conf

@@ -10,7 +10,7 @@ SOC_FAMILY = "mxs:mx28"

-UBOOT_CONFIG ??= "sd"

+UBOOT_CONFIG ??= "nand"

UBOOT_CONFIG[sd] = "mx28evk_config,sdcard"

UBOOT_CONFIG[nand] = "mx28evk_nand_config,ubifs"

UBOOT_CONFIG[sd-auart-console] = "mx28evk_auart_console_config,sdcard"

@@ -19,7 +19,7 @@ KERNEL_IMAGETYPE = "uImage"

SDCARD_ROOTFS ?= "${DEPLOY_DIR_IMAGE}/${IMAGE_NAME}.rootfs.ext3"

-IMAGE_FSTYPES ?= "tar.bz2 ext3 uboot.mxsboot-sdcard sdcard"

+IMAGE_FSTYPES ?= "tar.bz2 ext3 uboot.mxsboot-sdcard sdcard sb"

I built using bitbake core-image-minimal, but unfortunately this gave a build error partway and only one relevant file was generated: u-boot-imx28evk.sb

I then modified the ucl.xml in MfgTool to the following:

  <LIST name="Singlechip NAND" desc="Install on singlechip NAND">

    <CMD type="boot" body="Recovery" file="updater_ivt.sb" timeout="60">Booting Update Firmware.</CMD>

    <CMD type="find" body="Updater" timeout="180"/>

    <CMD type="push" body="mknod class/mtd,mtd0,/dev/mtd0"/>

    <CMD type="push" body="mknod class/mtd,mtd1,/dev/mtd1"/>

    <CMD type="push" body="mknod class/misc,ubi_ctrl,/dev/ubi_ctrl"/>

    <CMD type="push" body="$ flash_eraseall /dev/mtd0">Erasing rootfs partition 0</CMD>

    <CMD type="push" body="$ flash_eraseall /dev/mtd1">Erasing rootfs partition 1</CMD>

    <CMD type="push" body="send" file="files/u-boot-imx28evk.sb" >Sending Firmware</CMD>

    <CMD type="push" body="$ kobs-ng init $FILE">Flashing firmware</CMD>

    <CMD type="push" body="$ echo Update Complete!">Done</CMD>

  </LIST>

In hindsight the ubi_ctrl is probably not necessary since I don't load a root file system at this point.

I am also curious about nand flash erase. I would actually prefer to erase the entire /dev/mtd and not just a partition of it. Then again, I am uncertain where the NAND partition table is stored. Anyone who knows, please write a reply telling me. My current theory is that the NAND partition table only exists in the form of kernel parameters and stored in the environment part defined by mtdparts in u-boot.

At this point I set the i.mx28evk jumpers to boot from NAND and I get my u-boot prompt. Since my build earlier had failed I went back and changed machine config:

-IMAGE_FSTYPES ?= "tar.bz2 ext3 uboot.mxsboot-sdcard sdcard"

+IMAGE_FSTYPES ?= "tar.bz2 ext3 uboot.mxsboot-sdcard sdcard ubifs"

And built using bitbake core-image-minimal again.

Now it was time to play around with u-boot. I placed the generated uImage--2.6.35.3-r45-imx28evk-20140818140121.bin on a FAT formatted memory stick.

In u-boot i wrote the default mtdparts using mtdparts default and saveenv. Then I loaded the kernel into memory from the USB stick and wrote it to NAND.

usb start

fatls usb 0:1

fatload usb 0:1 0x40008000 uimage--2.6.35.3-r45-imx28evk-20140818140121.bin

nand erase 0x00400000 0x00400000 (last is size)

nand write 0x40008000 0x00400000 0x00400000 (last is size)

The load address 0x40008000 was obtained by running the following command from the build directory:

tmp/sysroots/x86_64-linux/usr/bin/uboot-mkimage  -l tmp/deploy/images/imx28evk/uImage--2.6.35.3-r45-imx28evk-20140818140121.bin

Image Name:   Linux-2.6.35.3-maintain+yocto+gb

Created:      Mon Aug 18 16:05:09 2014

Image Type:   ARM Linux Kernel Image (uncompressed)

Data Size:    2613036 Bytes = 2551.79 kB = 2.49 MB

Load Address: 40008000

Entry Point:  40008000

Now when the kernel is written to the NAND flash I setup the boot and save using the following commands

setenv bootcmd 'nboot 0x40008000 0 0x00400000; bootm'

saveenv

And now I can simply execute boot or reset the board to test:

U-Boot 2014.01 (Aug 18 2014 - 13:55:32)

CPU:   Freescale i.MX28 rev1.2 at 454 MHz

BOOT:  NAND, 3V3

DRAM:  128 MiB

NAND:  128 MiB

MMC:   MXS MMC: 0

Video: MXSFB: 'videomode' variable not set!

In:    serial

Out:   serial

Err:   serial

Net:   FEC0 [PRIME], FEC1

Hit any key to stop autoboot:  0

And the kernel is being loaded from NAND! Happy face!

Loading from nand0, offset 0x400000

   Image Name:   Linux-2.6.35.3-maintain+yocto+gb

   Created:      2014-08-18  14:05:09 UTC

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    2613036 Bytes = 2.5 MiB

   Load Address: 40008000

   Entry Point:  40008000

## Booting kernel from Legacy Image at 40008000 ...

   Image Name:   Linux-2.6.35.3-maintain+yocto+gb

   Created:      2014-08-18  14:05:09 UTC

   Image Type:   ARM Linux Kernel Image (uncompressed)

   Data Size:    2613036 Bytes = 2.5 MiB

   Load Address: 40008000

   Entry Point:  40008000

   Verifying Checksum ... OK

   XIP Kernel Image ... OK

Starting kernel ...

And crash! Sad face! But there is no rootfs in place which I am certain is causing the crash so now it is time to setup that.

undefined instruction

pc : [<40008010>]          lr : [<47f38440>]

sp : 47b32d70  ip : 00000000     fp : 00000000

r10: 00000000  r9 : 47b32f38     r8 : 47b417dc

r7 : 00000000  r6 : 40008000     r5 : 47f9f724  r4 : 00000000

r3 : 47b32fe0  r2 : 40000100     r1 : 000009e3  r0 : 47b32fe0

Flags: nZCv  IRQs off  FIQs off  Mode SVC_32

Resetting CPU ...

So now obviously the next step is the ubifs file and then I fill have to poke at TFTP to not be dependant on a USB thumb for transferring images.

5,053件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Can you share the error you are getting? Just like you said, it is very probable that the lack of the rootfs is causing that problem.

I do not know that if it is possible to generate a .sb file that only includes Linux, that way you can boot directly to Linux and get rid of U-Boot.

Best Regards,

Alejandro

0 件の賞賛
返信
5,054件の閲覧回数
persmitt
Contributor III

First of all, the error message is not hampering me in any way, so don't spend any time on it for my sake.

The setup I am trying to achieve is to use MfgTool to get U-Boot in place and after that use my own tools for communicating with U-Boot over the debug port.

I had just assumed that if I wanted .sb files I just set sb as a target and the files that could be generated would be. And since I got my U-Boot sb file I am very happy.

Since I did get everything I wanted I have not looked closely at the error and tried to debug it so it could be trivial. Just putting it out there to avoid wearing a dunce cap later on ;-)

When building the rootfs I get the following error (the referenced log file is attached):

ERROR: Error executing a python function in /home/per/work/fsl-community-bsp/sources/poky/meta/recipes-core/images/core-image-minimal.bb:

The stack trace of python calls that resulted in this exception/failure was:

File: 'do_rootfs', lineno: 17, function: <module>

    0013:    # generate final images

    0014:    create_image(d)

    0015:

    0016:

*** 0017:do_rootfs(d)

    0018:

File: 'do_rootfs', lineno: 14, function: do_rootfs

    0010:    # generate rootfs

    0011:    create_rootfs(d)

    0012:

    0013:    # generate final images

*** 0014:    create_image(d)

    0015:

    0016:

    0017:do_rootfs(d)

    0018:

File: '/home/per/work/fsl-community-bsp/sources/poky/meta/lib/oe/image.py', lineno: 329, function: create_image

    0325:        execute_pre_post_process(self.d, post_process_cmds)

    0326:

    0327:

    0328:def create_image(d):

*** 0329:    Image(d).create()

    0330:

    0331:if __name__ == "__main__":

    0332:    """

    0333:    Image creation can be called independent from bitbake environment.

File: '/home/per/work/fsl-community-bsp/sources/poky/meta/lib/oe/image.py', lineno: 307, function: create

    0303:        execute_pre_post_process(self.d, pre_process_cmds)

    0304:

    0305:        self._remove_old_symlinks()

    0306:

*** 0307:        image_cmd_groups = self._get_imagecmds()

    0308:

    0309:        for image_cmds in image_cmd_groups:

    0310:            # create the images in parallel

    0311:            nproc = multiprocessing.cpu_count()

File: '/home/per/work/fsl-community-bsp/sources/poky/meta/lib/oe/image.py', lineno: 277, function: _get_imagecmds

    0273:                localdata.setVar('OVERRIDES', '%s:%s' % (type, old_overrides))

    0274:                bb.data.update_data(localdata)

    0275:                localdata.setVar('type', type)

    0276:

*** 0277:                cmds.append("\t" + localdata.getVar("IMAGE_CMD", True))

    0278:                cmds.append(localdata.expand("\tcd ${DEPLOY_DIR_IMAGE}"))

    0279:

    0280:                if type in cimages:

    0281:                    for ctype in cimages[type]:

Exception: TypeError: cannot concatenate 'str' and 'NoneType' objects

ERROR: Function failed: do_rootfs

ERROR: Logfile of failure stored in: /home/per/work/fsl-community-bsp/sbtest/tmp/work/imx28evk-poky-linux-gnueabi/core-image-minimal/1.0-r0/temp/log.do_rootfs.3351

ERROR: Task 7 (/home/per/work/fsl-community-bsp/sources/poky/meta/recipes-core/images/core-image-minimal.bb, do_rootfs) failed with exit code '1'

0 件の賞賛
返信
5,054件の閲覧回数
persmitt
Contributor III

The problem is that the final hardware target does not have an SD card reader, only a NAND flash so I started searching for ways to make a NAND image. I found the following thread: To make NAND image by Yocto. which discusses the making of a NAND image but it differs from my requirements since the author is looking to use a direct NAND programmer and not MfgTool. I have no direct preference how to program the NAND and only want to find the smoothest way to do it. I have played around with MfgTool enough that I get it to download the special upgrade-Linux firmware into RAM. At this point I would have to supply a file to be flashed to NAND.

 

To generate such an image I have tried the following modifications to source/meta-fsl-arm:

diff --git a/conf/machine/imx28evk.conf b/conf/machine/imx28evk.conf

index d4f1ad6..2b6939e 100644

--- a/conf/machine/imx28evk.conf

+++ b/conf/machine/imx28evk.conf

@@ -10,7 +10,7 @@ SOC_FAMILY = "mxs:mx28"

-UBOOT_CONFIG ??= "sd"

+UBOOT_CONFIG ??= "nand"

UBOOT_CONFIG[sd] = "mx28evk_config,sdcard"

UBOOT_CONFIG[nand] = "mx28evk_nand_config,ubifs"

UBOOT_CONFIG[sd-auart-console] = "mx28evk_auart_console_config,sdcard"

@@ -19,7 +19,7 @@ KERNEL_IMAGETYPE = "uImage"

SDCARD_ROOTFS ?= "${DEPLOY_DIR_IMAGE}/${IMAGE_NAME}.rootfs.ext3"

-IMAGE_FSTYPES ?= "tar.bz2 ext3 uboot.mxsboot-sdcard sdcard"

+IMAGE_FSTYPES ?= "tar.bz2 ext3 ubifs"

 

0 件の賞賛
返信
5,054件の閲覧回数
persmitt
Contributor III

Then I created the images using: bitbake core-image-minimal. This only yielded the following files:

 

persm@mewmew:~/work/fsl-community-bsp/build/tmp/deploy/images/imx28evk$ ls -la

total 47412

drwxrwxr-x 2 persm persm     4096 aug 15 14:25 .

drwxrwxr-x 3 persm persm     4096 aug 15 14:23 ..

-rw-r--r-- 1 persm persm 67108864 aug 15 14:25 core-image-minimal-imx28evk-20140815110253.rootfs.ext3

-rw-r--r-- 1 persm persm     1286 aug 15 14:25 core-image-minimal-imx28evk-20140815110253.rootfs.manifest

-rw-r--r-- 1 persm persm  6432958 aug 15 14:25 core-image-minimal-imx28evk-20140815110253.rootfs.tar.bz2

-rw-r--r-- 1 persm persm 15998976 aug 15 14:25 core-image-minimal-imx28evk-20140815110253.rootfs.ubifs

lrwxrwxrwx 1 persm persm       54 aug 15 14:25 core-image-minimal-imx28evk.ext3 -> core-image-minimal-imx28evk-20140815110253.rootfs.ext3

lrwxrwxrwx 1 persm persm       58 aug 15 14:25 core-image-minimal-imx28evk.manifest -> core-image-minimal-imx28evk-20140815110253.rootfs.manifest

lrwxrwxrwx 1 persm persm       57 aug 15 14:25 core-image-minimal-imx28evk.tar.bz2 -> core-image-minimal-imx28evk-20140815110253.rootfs.tar.bz2

lrwxrwxrwx 1 persm persm       55 aug 15 14:25 core-image-minimal-imx28evk.ubifs -> core-image-minimal-imx28evk-20140815110253.rootfs.ubifs

-rw-rw-r-- 2 persm persm   784435 aug 15 14:23 modules--2.6.35.3-r45-imx28evk-20140815110253.tgz

lrwxrwxrwx 1 persm persm       49 aug 15 14:23 modules-imx28evk.tgz -> modules--2.6.35.3-r45-imx28evk-20140815110253.tgz

-rw-r--r-- 2 persm persm      294 aug 15 14:24 README_-_DO_NOT_DELETE_FILES_IN_THIS_DIRECTORY.txt

lrwxrwxrwx 1 persm persm       48 aug 15 14:23 uImage -> uImage--2.6.35.3-r45-imx28evk-20140815110253.bin

-rw-r--r-- 2 persm persm  2612216 aug 15 14:22 uImage--2.6.35.3-r45-imx28evk-20140815110253.bin

lrwxrwxrwx 1 persm persm       48 aug 15 14:23 uImage-imx28evk.bin -> uImage--2.6.35.3-r45-imx28evk-20140815110253.bin

 

0 件の賞賛
返信
5,053件の閲覧回数
persmitt
Contributor III

As far as I can tell I have a ubifs file for the rootfs file system and thats it. Maybe I don't need to have all files as ubifs since I am using MfgTool but I don't know. I also seem to lack a u-boot image and the actual kernel image seems to be just a standard uImage. Can I simply place the kernel image in the NAND just like that, and if so how does it deal with a potential bad sector there?

0 件の賞賛
返信
5,053件の閲覧回数
persmitt
Contributor III

If anyone have any tips, advice or even a guide how to build a NAND image in Yocto and get it to run on the nand flash on the imx28evk I would be really grateful.

Many thanks and apologies for the horrible structure of messages.

/Per Smitt

0 件の賞賛
返信