Question about how to automate power-up sequence.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Question about how to automate power-up sequence.

跳至解决方案
809 次查看
hikaruuruno
Contributor III

Hi Community,

We are planning to make a custom board with DCDC_BATT source only configuration which will power-up automatically when the power is supplied.

There are description in the documents of i.MX28 that in case of DCDC_BATT source only configuration, PSWITCH pin must be around MID level for 100ms to power up the IC.

Also, there is a description that "A MID LEVEL PSWITCH state can be generated by connecting the VDDXTAL output of the SoC to PSWITCH through a switch."

I suppose the part "through a switch" is to control power-up manually.

So, is there no problem to connect PSWITCH and VDDXTAL directly to automate power-up?

I could not find the exact same question in the community but if there is one and I just missed it, please redirect me to it.

Thank you in advance,

Hikaru

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
703 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hikaru

you are right, one can connect VDDXTAL via 1K to PSWITCH.

This triggers the startup automatically.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
704 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Hikaru

you are right, one can connect VDDXTAL via 1K to PSWITCH.

This triggers the startup automatically.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复