Queries on IMX6ULL processor GPIO pin.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Queries on IMX6ULL processor GPIO pin.

1,578 Views
ramesh6663
Contributor III

Hi,

  Could you please let me know the Maximum drive current of IMX6ULL GPIO pin from Processor?  I believe its >10mA.

 So please confirm 

Thanks 

Labels (1)
0 Kudos
Reply
3 Replies

1,130 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The GPIO buffer load capacity is not specified in units of current. It is specified in terms of buffer drive strength or output impedance. For example, refer to the Section "GPIO Output Buffer Impedance" of the i.MX 6ULL Data Sheet(s).

 

IBIS models may be used to estimate current.

 

https://community.nxp.com/message/395489 

 

Also, the total load current and power dissipation should be taken into account when calculating the GPIO power budget.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,130 Views
ramesh6663
Contributor III

Thanks Yuri,

  I am just using Ohms law to determine the current for the GPIO when its 3.3V IO logic, Drive current form 20mA to 140mA as per "4.8.1 Single Voltage GPIO Output Buffer Impedance" in the datasheet. Am i right?

And we are going to use GPIO in sourcing power to the LED for Indication use case.

Thanks,RK

0 Kudos
Reply

1,130 Views
Yuri
NXP Employee
NXP Employee

Hi,

  You should take into account LED volt ampere characteristic.

https://community.nxp.com/message/381665 

 

Regards,

Yuri.

0 Kudos
Reply