Hello, I am using the IMX7ulpevk board with kernel linux-imx on tag rel_imx_5.4.24_2.1.0.
Is it possible to access the squad spi flash from Linux for modifications ? Does that only need change in the device tree ?
Louson
解決済! 解決策の投稿を見る。
Hi Louson
examples of access can be found on
https://wiki.phytec.com/pcm061/using-peripherals/qspi-nor-flash
One can try with EVK i.MX 7ULP EVK Linux Binary Demo Files
for qspi use dts file: imx7ulp-evk-qspi.dts
Best regards
igor
suppressed
Hi Louson
examples of access can be found on
https://wiki.phytec.com/pcm061/using-peripherals/qspi-nor-flash
One can try with EVK i.MX 7ULP EVK Linux Binary Demo Files
for qspi use dts file: imx7ulp-evk-qspi.dts
Best regards
igor
Hello,
Thanks fo this quick answer. However, there is no qspi devive tree in this 5.4.47 release. Is's been missing for imx7ulp since the kernel is 5.x.
The linked dts is from the u-boot device tree, which is not exactly compatible with linux's. I'll try again though
Louis
Hi Louis
qspi is not used in linux because it is used by M4 SDK (folder ../driver_examples/qspi)
https://mcuxpresso.nxp.com/en/welcome
Best regards
igor