Qt 5.12 build on Yocto 2.0.3 jethro, for imx6q

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Qt 5.12 build on Yocto 2.0.3 jethro, for imx6q

1,104 次查看
sergei_p
Contributor III

Hello,

We have a IMX6Q BSP based on Yoct 2.0.3 Jethro, with meta-qt5 v 5.5.1. Now, we are asked to upgrade to meta-qt5 v5.12, in context of the same Yocto 2.0.3.

Is there someone who tried to upgrade to the newest meta-qt with some older IMX Yocto distributions? Is it doable?

Or should we consider from the start to switch to the latest IMX 4.14.78 first, and then try to upgrade to meta-qt5 5.12 from there?

Any thoughts are welcome.

Regards,

Sergei

标签 (3)
0 项奖励
回复
1 回复

893 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Sergei,

The problem is that  QT version 5.12 does not work even in 4.14.78, you have to check it with the community.

FSL Community BSP 

Regards

0 项奖励
回复