Hello, I use i.MX6 sabre platform and fsl-yocto-3.10.53-1.1.0 BSP.
There is qt5everywheredemo-1.0 and some domos in BSP and it works fine for building and running.
Then I want to deploy some custom qt project, but i.MX_Linux_User's_Guide says running demos only.
Is there some references for custom qt project?
For example, how to import qtcreator's project?
I followed this article and made a excutable binary but it can not run in board with this message.
Setup QT Creator with Yocto Build
-------------------------------
QIconvCodec::convertFromUnicode: using Latin-1 for conversion, iconv_open failed
QIconvCodec::convertToUnicode: using Latin-1 for conversion, iconv_open failed
untitled: cannot connect to X server
-------------------------------
And in host PC, when tring to make iconv below error is printed.
-------------------------------
$ bitbake libiconv
ERROR: Multiple .bb files are due to be built which each provide virtual/libiconv (/var/work/i.mx6/fsl-release-bsp/imx-3.10.53/sources/poky/meta/recipes-support/libiconv/libiconv_1.14.bb /var/work/i.mx6/fsl-release-bsp/imx-3.10.53/sources/poky/meta/recipes-core/eglibc/eglibc_2.19.bb).
This usually means one provides something the other doesn't and should.
-------------------------------
Solved! Go to Solution.
Here is a document on community regarding QT Creator installation in Yocto:
https://community.freescale.com/message/339555#339555
And here is regarding installation it in Ubuntu:
https://community.freescale.com/docs/DOC-94252
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Here is a document on community regarding QT Creator installation in Yocto:
https://community.freescale.com/message/339555#339555
And here is regarding installation it in Ubuntu:
https://community.freescale.com/docs/DOC-94252
Have a great day,
Victor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------