Does anyone have experience getting the power consumption of the QSB down?
Our application does not need any of the audio or video functionality.
At the LINUX prompt the board draws 380 to 500 mA from the 5V main supply. Thats about 2W to 2.5W.
The Freescale app note says that LINUX can draw about 160 mW while playing an MP3 file from SD,
Is there some low power demo code I can run and/or does anyone have experiene reducing the power consumption of the QSB?
Thanks.
-Ted
If I knew how to disable these systems, then I would do so and then read the current. I'm just a hardware guy on this project.
(I was hoping someone had made some measurements and/or computations already.)
-Ted
OK, I now understand that cpufreq-info is LINUX command that will provide the current frequency/power trade off info, but I'm more interested in what happens when the video and audio stuff is disabled or removed and when the power supplies are designed more efficiently than in the QSB. How close can I get the 2W that the QSB boots up to in LINUX down to the 160 mW listed in the App note for just processing MP3 video from an SD card. That's a BIG gap!
-Ted