Pull-up/down resistor enable iMX Config Tool v9.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Pull-up/down resistor enable iMX Config Tool v9.0

跳至解决方案
2,346 次查看
LaurentL
Contributor I

Hi,

I am trying to enable pull-up or down resistor with the iMX config tool v9.0.

Once routed, there is a field named "Pull Resistors Enable Field" which allows to select "Enabled", "Disabled", "No init", etc. But I cannot figure out were to set if I want to configure it as pull-up or down. I saw in previous version of the software some screenshot showing a "Pull Select" section allowing to define it.

Am I missing something ?

Thank you

0 项奖励
回复
1 解答
2,274 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

It is a display limitation, please see the next property "Pull Resistors Enable Field" -> "Control IO ports PS", it means Pull Select Control IO, you can set Pull Up/Down by selecting it. Please find the image attached.

 

It will be aligned to the legacy name in the next version of the Tool to avoid any misunderstanding.

 

Hope it helps!

 

BR,

Ivan.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,307 次查看
LaurentL
Contributor I

Hello,

I just checked out some other processors and it seems the one I am trying to use (IMX8M Nano) does not enable those fields.

What should I do to configure pull-up or down resistors on the processor IO ? Is there any other way of configuring them ? I may be missing something here.

Best regards,

Laurent

0 项奖励
回复
2,275 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

It is a display limitation, please see the next property "Pull Resistors Enable Field" -> "Control IO ports PS", it means Pull Select Control IO, you can set Pull Up/Down by selecting it. Please find the image attached.

 

It will be aligned to the legacy name in the next version of the Tool to avoid any misunderstanding.

 

Hope it helps!

 

BR,

Ivan.

0 项奖励
回复
2,323 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

 

I just have downloaded the V9 version and by default, it has available the "Pull-up / Down config field", please see below:

IvanRuiz_0-1616015288176.png

 

Please check that the pin of your interest supports this functionality.

 

BR,

Ivan.

 

0 项奖励
回复