Porting uboot 2016 to uboot 2018 imx6ull

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Porting uboot 2016 to uboot 2018 imx6ull

531 Views
deepanrajanbara
Contributor IV

Hi,

As we are trying to port uboot to the latest version. after Doing the changes which are similar to that of the uboot 2016. The board doesnt boot.

Please help us to debug the uboot. Is there any changes need to be done w.r.t uboot 2018.

Thank you,

Deepanraj

Labels (1)
0 Kudos
Reply
1 Reply

494 Views
igorpadykov
NXP Employee
NXP Employee

Hi Deepanraj

nxp has uboot ver. 2018 on its source.codeaurora.org/external/imx  repository

mx6ullevk\freescale\board - uboot-imx - i.MX U-Boot 

For porting one can use Porting Guide included in Linux 4.19.35_1.1.0 Documentation

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply