BSP is linux L3.14.28_1.0.0-ga
MACHINE=imx6sxsabresd source fsl-setup-release.sh -b build-wayland -e wayland
bitbake fsl-image-qt5
Porting QT4.8.6
Environmental variable:
harry@mh:~/NfsRoot/etc$ vim qt4_env
1 #!/bin/sh
2
3 if [ -c /dev/input/event0 ]; then
4 INPUT_PATH=/dev/input
5 else
6 INPUT_PATH=/dev
7 fi
8
9 export TSLIB_TSDEVICE=/dev/input/event1
10 export TSLIB_CONFFILE=/etc/ts.conf
11 export TSLIB_PLUGINDIR=/lib/ts
12 export TSLIB_CALIBFILE=/etc/pointercal
13 export QTDIR=/usr/qt4_embedded_arm/
14 export PATH=$QTDIR/bin:$PATH
15 export LD_LIBRARY_PATH=$QTDIR/lib
16 export QWS_MOUSE_PROTO="Tslib:$INPUT_PATH/event1"
17 export QWS_KEYBOARD=TTY:/dev/tty1
18 export QT_QWS_FONTDIR=$QTDIR/lib/fonts/
19
20 export QWS_DISPLAY="LinuxFB:/dev/fb0"
22
23 export KDEDIR=/opt/kde
24
25 export HOME=/root
./test -qws
Move the mouse
App is not on the table,
but app is running.
I don't know how to show it
Running in the foreground
Use the mouse to operate it
Qt required X11 back end and necessary EPD update routines for running the sample applications.