Porting KSZ9031RN to imx6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Porting KSZ9031RN to imx6

ソリューションへジャンプ
1,640件の閲覧回数
bastien
Contributor I

Hello !

I am working on imx6 processor custom board, i added the KSZ9031 phy Ethernet on the board.

Recommendations in the post Porting KSZ9031 to i.MX BSP gives the phy side schematic only.

I am not sure if i correctly connected the RGMII_INT pin (p38) to the imx6 (see attached pictures).

Thank you

BR

 

0 件の賞賛
返信
1 解決策
1,625件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

I use this PHY in a i.MX7D board design. I connected this INT pin to a gpio in case we may check the INT output signal in future. For normal using, we don't need to care this INT signal.

 

pin.png

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,626件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

I use this PHY in a i.MX7D board design. I connected this INT pin to a gpio in case we may check the INT output signal in future. For normal using, we don't need to care this INT signal.

 

pin.png

0 件の賞賛
返信