Port of BCMDHD code modifications from i.MX7 to i.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Port of BCMDHD code modifications from i.MX7 to i.MX6

1,210 Views
CodeWarrior4_2M
Contributor II

Is there any reason to not port the following code modification on i.mx6?

linux-2.6-imx.git - Freescale i.MX Linux Tree

I am on the imx_3.14.38_6ul_ga and would expect the same type of update for the dts file like: imx6ul-14x14-evk.dts

Thanks for your comment

Labels (4)
0 Kudos
Reply
2 Replies

962 Views
igorpadykov
NXP Employee
NXP Employee

Hi 79

one can try attached patch.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

962 Views
mickaeltoumi
Contributor III

Thank Igor.

0 Kudos
Reply