Hi,
I am getting really poor performance on the i.MX 53 with Qt4.7.4 and the hellogl_es2 example.
The fps is showing about 13 fps. I installed Qt with the X-server.
The screen resolution is 1024x786.
Any ideask, why the performance is so poor?
HI DD1z,
could you fix the problem?. I'm having the same issue, even worst, just 6fps.
Regards
on i.MX51 amd-gpu-bin-mx51
Could you run Qt over the frame buffer with GPU enabled?. I had no success and in several posts it is said you need to enable a specific plugin.
Thanks in advance,
Which screen driver are you using?
I use without X11 libs and it's working fine.