Play video in i.mx6 with mplayer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Play video in i.mx6 with mplayer

1,493 Views
zc_tee
Contributor III

Hi all,

I would like to utilize the hardware decoder in the i.mx6 to play mp4 video file using mplayer.

May i know what is the command to specific the mplayer to play the video using hardware decoder?

I tried "mplayer video.mp4", and it seems like it's playing the video using software decoder, cause the CPU usage shoot up to 100%.

Please help. Thanks.

Regards,

ZC

Labels (4)
0 Kudos
Reply
1 Reply

771 Views
Yuri
NXP Employee
NXP Employee

Hello,

  The mplayer uses standard software codecs. Hardware options may
be used via gstreamer or gplay, that is based on gstreamer.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply