Partial Image Authentication in HAB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Partial Image Authentication in HAB

556件の閲覧回数
norratheprattan
Contributor I

I'm not sure if my previous question has been noticed since I put it in a comment. So I'll put it here instead.

Based on my understanding of HAB and HAB uImage Layout, uImage is authenticated as a whole by u-boot. and it seems to be the case for example API provided in a document.

Is there a code (and/or is it possible at all in HAB) for authenticating only a partial uImage since some parts of our image (at least at the end) should support a code update.

Thanks,

ラベル(3)
0 件の賞賛
返信
1 返信

481件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Basically boot ROM HAB API is used just to check an area in memory,

so, if customer's uImage can be split into two parts - it is possible to sign

only one of them (based on uImage memory layout).  

Have a great day,

Yuri

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

0 件の賞賛
返信