How to configure MFGTools on IMX7

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure MFGTools on IMX7

1,490 Views
864535720
Contributor II

hi:

   I have a board, Its chip model is a MCIMX7D7DVM10SD .

  • I've tried a lot of MFGTools,But it didn't work,and  I saw a post of BBS(mfgtools to imx7d ), which recommended a tool version. When I tried it, there was still no effect. The problem I encountered was how to configure McImx7ddvm10sd,When I changed the model of the chip, as in your manual, "chip = MX6DL Linux Update" changed to"chip = MX7D Linux Update", the tool could not run.

  • pastedImage_18.png
  • pastedImage_19.png
  • pastedImage_20.png
  • I dont change ucl。
Labels (1)
0 Kudos
Reply
5 Replies

1,139 Views
igorpadykov
NXP Employee
NXP Employee

Hi 其东 

for using MCIMX7D7DVM10SD there is no need for changing the model of the chip,

please try to click on appropriate *.vbs file. Check that board USB_OTG_ID signal is high.

Below mfg tool presentation which may be helpful:

AMF-ACC-T1652 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,139 Views
864535720
Contributor II

hi igorpadykov

   When I am using MFGTools, should I install the driver of MFGTools first, because after I connect to OTG,My PC did not detect that the device was connected.

  • How do I install the driver

0 Kudos
Reply

1,139 Views
igorpadykov
NXP Employee
NXP Employee

when using MFGTools, windows uses native hid driver when detecting board, so no

need for additional drivers for board.

Best regards
igor

0 Kudos
Reply

1,139 Views
igorpadykov
NXP Employee
NXP Employee

no additional drivers are needed, suggest to

check that board USB_OTG_ID signal is high.

Best regards
igor

0 Kudos
Reply

1,139 Views
864535720
Contributor II

OK,My problem has been solved。

The solution is:把SD卡取下来,然后连接OTG,给开发板上电,这个时候通过MFGTools去查看,会发现开发板是可以识别的,然后再把SD卡给插上去,点击start,就可以开始下载程序。(注意:我的开发板上没有emmc、nand flash等。然后就是我的boot_mode设置其实是没有效果的。为啥没有效果,目前也没有彻底明白。只有问开发板了!)

0 Kudos
Reply