PIMX8QM6AVUFFAB 的SCU_WDOG_OUT输出波形

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

PIMX8QM6AVUFFAB 的SCU_WDOG_OUT输出波形

1,232 次查看
3217768732
Contributor I

After powered up  ,the IMX8Q's BB50 (SCU_WDOG_OUT) ouput like that ,cann't detect usb ,and I tie this pin to WDI belonged to  pmic ,and this waveform make PMIC reset at 3,243Hz,can anyone know how to solve this problem ,thx a lotpastedImage_1.png

标记 (1)
0 项奖励
回复
5 回复数

1,062 次查看
jimmychan
NXP TechSupport
NXP TechSupport

For your reference : https://community.nxp.com/docs/DOC-343102 

“Note:

In default SCFW, it had already used internel watchdog to make sure SCFW is always running, if SCFW is built as no debug version (M=0 D=0), all SCFW halt will cause SOC reset. And if hardware had connected the SCU_WDOG_OUT pin from iMX8QXP to PMIC's WDI pin, then during SOC reset, the PMIC will also do hard reset to make a POR reboot for the whole system.”

0 项奖励
回复

1,062 次查看
3217768732
Contributor I

think u ,but the first time to supply power for IMX8,even never detect HID ,none enable internel watchdog,how can I disable the watchdog?

0 项奖励
回复

1,062 次查看
jimmychan
NXP TechSupport
NXP TechSupport

Do you mean your board cannot go to the USB download mode?

0 项奖励
回复

1,062 次查看
3217768732
Contributor I

yes,first time to power up

cann't detect USB HID,cann't goto download mode

two pgoods from PMICs are high ,but no voltage CPU0 CPU1 GPU0 GPU1

0 项奖励
回复

1,062 次查看
jimmychan
NXP TechSupport
NXP TechSupport

What is the boot mode pin setting on your board?

0 项奖励
回复