Dear community,
We have been developing our product with PF3000.
I have a question about LICELL Coin cell charger behavior.
PF3000 has the coin cell charger functions via LICELL pin.
[Question]
If the Coin cell charger voltage which is set by VCOIN[2:0] register is lower than attached Coin cell voltage,
Is there any problem ?
I worry about that the flowing current to PF3000 from the Coin cell feeds a damage for internal circuit. (in the case of COINCHEN = 1)
Best Regards,
Koichi Sakagami
Solved! Go to Solution.
Hi Koichi
> If the Coin cell charger voltage which is set by VCOIN[2:0] register is lower than attached Coin cell voltage,
> Is there any problem ?
no problem, as coin cell charger circuit is implemented in such way
so coin cell can not feed backward current to charger circuit .
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Koichi
> If the Coin cell charger voltage which is set by VCOIN[2:0] register is lower than attached Coin cell voltage,
> Is there any problem ?
no problem, as coin cell charger circuit is implemented in such way
so coin cell can not feed backward current to charger circuit .
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------