PCIe Endpoint Doorbell or Interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIe Endpoint Doorbell or Interrupt

5,926 Views
carlpii
Contributor I

It is common for a PCIe add-in card to have a "doorbell" register or similar functionality (eg, a queue tail pointer) that the host system can write to start an I/O operation.  I haven't found a way to trigger an ARM interrupt as a result of an inbound PCIe write transaction with the i.MX6 operating in endpoint mode.  I'm currently stuck polling on memory locations which is a really ugly solution.  Is there a way to implement this type of behavior that doesn't rely on polling?

Thanks,

-Carl

0 Kudos
Reply
1 Reply

3,757 Views
Yuri
NXP Employee
NXP Employee

Hello,


The following discussion - hope - helps.

https://community.nxp.com/t5/i-MX-Processors/Endpoint-Interrupt-via-PCIe/m-p/250595

 

Regards,
Yuri.

 

0 Kudos
Reply