Hello,
I have a multimedia software based on OpenMAX IL that runs on Linux.
I'd like to know if there any support for OpenMAX from i.MX drivers so that I can easily port this software to i.MX platform?
Thanks.
Hi Yevhen
i.mx extended multimedia feature package provides support
for OMXPlayer framework for android, not for linux.
Board Support Packages (27)
IMX6-L500-100-ANDROID-SOURCE-BSP (REV L5.0.0_1.0.0)
i.MX 6Quad, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo i.MX 6Sololite and
i.MX6SX Android L5.0.0_1.0.0 BSP, Source Code for BSP and Codecs.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------