Hi NXP FAEs:
I intend to online program NOR flash on imx27 plateform board. I have the source package: FSL_ATK_SRC_STD_1_60 and reference manual: pdk10_imx_ATK_Std_RM.pdf on hand. I try to make up a build system to generate the bin file for the flash we used. I get an issue then.
The tool chain source: http://www.gnuarm.com/bu-2.17_gcc-4.1.1-c-c++_nl-1.14.0_gi-6.5.exe is not there any longer.
1. Do you have any way to help me to get the tool chain file?
2. Or do you have any software packages(such as arm-elf-tool) which can work on Ubuntu system?
Best Regards.
Johnson
why don't you try to use mx27 bsp? which includes the tool chain
<i.MX27 Product Development Kit|NXP >
focus on the "Board Support Packages"