Not able to driver high on UPLL_BYPCLK with ALT5 using i.mx25

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Not able to driver high on UPLL_BYPCLK with ALT5 using i.mx25

Jump to solution
898 Views
suzan
Contributor II

Hi,

I am working on iMX258. I want to drive high and low on UPLL_BYPCLK line. I

configured this line with ALT5 functionality (GPIO), Since there is no PAD

configuration register for this line my level change doesn't effect the environment.

How can I drive different level on the pin UPLL_BYPCLK (GPIO[16]).

Regards,

suzan


Labels (1)
0 Kudos
Reply
1 Solution
836 Views
jimmychan
NXP TechSupport
NXP TechSupport

According to the i.MX25RM Table 4-18, UPLL_BYPCLK is only DVS can be configured.

=======================

Hysteresis Enable—Disabled

Drive Strength—Nominal

Pull/Keep Enable—Disabled

Pull Up/Down Configuration—100 KΩ PU

Open Drain Enable—Disabled

Drive Voltage Select—CFG (3.3 V)

Pull/Keep Select—Keep

Slew Rate—FAST

=======================

By default, the DVS is 3.3V.

You can change the setting in (Offset 0x0434) (IOMUXC_SW_PAD_CTL_GRP_DVS_CRM)

Please check if you set it correct.

View solution in original post

0 Kudos
Reply
1 Reply
837 Views
jimmychan
NXP TechSupport
NXP TechSupport

According to the i.MX25RM Table 4-18, UPLL_BYPCLK is only DVS can be configured.

=======================

Hysteresis Enable—Disabled

Drive Strength—Nominal

Pull/Keep Enable—Disabled

Pull Up/Down Configuration—100 KΩ PU

Open Drain Enable—Disabled

Drive Voltage Select—CFG (3.3 V)

Pull/Keep Select—Keep

Slew Rate—FAST

=======================

By default, the DVS is 3.3V.

You can change the setting in (Offset 0x0434) (IOMUXC_SW_PAD_CTL_GRP_DVS_CRM)

Please check if you set it correct.

0 Kudos
Reply