Hi,
I am working with freescale's imx28 dev board and i cannot use my 1 GiB nand flash (MT29F8G09ABABA). I added lines as below to ~/ltib/rpm/BUILD/linux/drivers/mtd/nand/nand_device_info.c file;
/* * Type 2 */
static struct nand_device_info nand_device_info_table_type_2[] __initdata = {
.......
{
.end_of_table = false,
.manufacturer_code = 0x2c,
.device_code = 0xd3,
.cell_technology = NAND_DEVICE_CELL_TECH_SLC,
.chip_size_in_bytes = 1LL*SZ_1G,
.block_size_in_pages = 128,
.page_total_size_in_bytes = 4*SZ_1K + 224,
.ecc_strength_in_bits = 4,
.ecc_size_in_bytes = 512,
.data_setup_in_ns = 25,
.data_hold_in_ns = 15,
.address_setup_in_ns = 10,
.gpmi_sample_delay_in_ns = 6,
.tREA_in_ns = -1,
.tRLOH_in_ns = -1,
.tRHOH_in_ns = -1,
"MT29F8G08ABABA",
}
, {true}
};
and i prepare a sd card for booting. Then i booted my board and checked my mtd devices;
$ mtdinfo
Count of MTD devices: 0
Please help, I have no time
Regards,
Sinan
Maybe you could try this kind of setting:
{
...
.page_total_size_in_bytes = 4*SZ_1K + 218,
...
}
And: 512 KiB, 516096, 2008, 4096
With these settings I'm able to boot from NAND
So this is the only output you get when you reboot?
Yes
Are you sure you got a good kernel image loaded into NAND? How are you creating your kernel image?
Yes, I am sure that it is ok because i tried it with an another nand flash and it works.
Also i created it with ltib script;
$ ./ltib
$ ./ltib -p boot_stream.spec -f
In my opinion, LTIB does not support Open Nand devices well.(my flash has ONFI 2.1)
only outputs this : HTL0x8050100b
but my mtdinfo output as below:
root@freescale ~$ mtdinfo -a
Count of MTD devices: 2
Present MTD devices: mtd0, mtd1
Sysfs interface supported: yes
mtd0
Name: gpmi-nfc-0-boot
Type: nand
Eraseblock size: 524288 bytes, 512.0 KiB
Amount of eraseblocks: 40 (20971520 bytes, 20.0 MiB)
Minimum input/output unit size: 4096 bytes
Sub-page size: 4096 bytes
OOB size: 224 bytes
Character device major/minor: 90:0
Bad blocks are allowed: true
Device is writable: true
mtd1
Name: gpmi-nfc-general-use
Type: nand
Eraseblock size: 524288 bytes, 512.0 KiB
Amount of eraseblocks: 2008 (1052770304 bytes, 1004.0 MiB)
Minimum input/output unit size: 4096 bytes
Sub-page size: 4096 bytes
OOB size: 224 bytes
Character device major/minor: 90:2
Bad blocks are allowed: true
Device is writable: true
As you see, settings should be 512KiB, 516096, 2048, 4096 ?
Also, a hour ago I realized that if I boot from nand, it does not loaded linux from nand. But if I load the linux from mmc card, then I can access rootfs in the nand flash.
How can I solve this issue?
mtdinfo can give you lots of information about your NAND device. I use these settings on most of mine but it depends on your particular device. Use the mtdinfo output to check.
128KiB, 126976, 4096, 2048
Mike,
I have a question for you such that have you used ubifs for nand ? if yes, what are the ubifs parameters ?
PEB size:
LEB size:
Max LEB count:
Min I/O unit size:
I tried it with :
-> 512 KiB, 516096, 2048, 4096
-> 512 KiB, 516096, 4096, 4096
-> 512 KiB, 516096, 2008, 4096
but I can't boot from nand
Ok...some further info regarding the issue I mentioned above:
For my device, the ID_GET_MICRON_SIMUL_PROG() macro used in nand_device_info_fn_micron() (nand_device_info.c in rpm/BUILD/linux/drivers/mtd/nand) yields the value 0x01. As a result nand_device_info_table_type_7 is checked. However, the definition for the MT29F2G08 is in the _type_2 table. I don't know enough about the code/flash devices to determine if the macro or the table placement is the problem...
Regarding your issue though, I see that the "MT29F8G08FABWG" entry in the type 7 table is already associated with mfr code 0x2c and device code 0xd3, although some of your sizing information differs. I think some of the info at boot will help folks determine if it's something along the lines of lacking MTD support in your kernel, incorrect device parameters, etc.
Is the device detected at boot? The relevant lines from dmesg might help.
I had an issue with the MT29F2G08 not being detected at boot -- basically the code that probes for nand devices was looking for my device in the type_7 table instead of the type_2 table due to the contents of one of the ID bytes. I ended up moving the device info (similar to what you posted) to the type_7 table, and I was able to work with the flash device.
I'll check into more of the specifics when I have the code in front of me and let you know. :)