NXP IMX8M PLUS Yocto 5.15.32 BSP Build Fail on Ubuntu 18.04

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP IMX8M PLUS Yocto 5.15.32 BSP Build Fail on Ubuntu 18.04

Jump to solution
1,016 Views
woohyoungshin
Contributor II

 

Loading cache: 100% | | ETA: --:--:--
Loaded 0 entries from dependency cache.
Parsing recipes: 100% |###################################################################################################################################################################################| Time: 0:00:10
Parsing of 3236 .bb files complete (0 cached, 3236 parsed). 4787 targets, 524 skipped, 5 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies
NOTE: Multiple providers are available for virtual/opencl-icd (imx-gpu-viv, opencl-icd-loader)
Consider defining a PREFERRED_PROVIDER entry to match virtual/opencl-icd

 

 

Initialising tasks: 100% |################################################################################################################################################################################| Time: 0:00:05
Checking sstate mirror object availability: 100% |########################################################################################################################################################| Time: 0:00:08
Sstate summary: Wanted 2838 Local 0 Mirrors 0 Missed 2838 Current 363 (0% match, 11% complete)
NOTE: Executing Tasks
WARNING: imx-gpu-viv-1_6.4.3.p4.2-aarch64-r0 do_fetch: Failed to fetch URL 

 

 

what is the problem?

0 Kudos
Reply
1 Solution
903 Views
woohyoungshin
Contributor II

It is solved. thank you for ur regarding.

View solution in original post

3 Replies
976 Views
kunyichen
Contributor IV

Error message tell you fetch failed

'ERROR: imx-gpu-viv-1_6.4.3.p4.2-aarch64-r0 do_fetch: Bitbake Fetcher Error: FetchError('Unable to fetch URL from any source.', 'https://www.nxp.com/lgfiles/NMG/MAD/YOCTO//imx-gpu-viv-6.4.3.p4.2-aarch64.bin;fsl-eula=true')'

so check your network/proxy setting first

I tested the download uri is okay now

kunyichen_0-1698989082603.png

 

904 Views
woohyoungshin
Contributor II

It is solved. thank you for ur regarding.

981 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

For this version BSP the recommended minimum Ubuntu version is 20.04 or later.

0 Kudos
Reply