NVCC_PLL_OUT Supply rail of I.MX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NVCC_PLL_OUT Supply rail of I.MX6

928 Views
vigneshvasudeva
Contributor II

Hi,

We are using I.MX6 in one of our solutions and I need some clarification regarding "NVCC_PLL_OUT" rail.

In page 554 of IMX6DQRM, it is mentioned that the rail is generated from an internal LDO. Whereas in Sabre-SD board schematic, it is illustrated that the rail is generated using an External LDO.

imx6.png

Kindly refer to the above image for clarity and let me know whether the external LDO is needed.

Tags (3)
0 Kudos
Reply
2 Replies

691 Views
Yuri
NXP Employee
NXP Employee

   Generally, for performance, it is better using an external power supply for the PLL. Also, because

of some bugs in old silicon versions the external PLL supply was implemented on the SDP / SDB

designs.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

691 Views
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.g. i.MX Community ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community.

0 Kudos
Reply