We are capturing NTSC video using an e-consystems e-CAMNT_MX53x (using tvp5147m1_tvin.ko) plugged into an i.MX53 Quick Start Board.
We run the e-consystems demo program selecting option 2 for NTSC and option 5 to combine the odd and even fields.
The field order is flipped, I think it is related to analog PAL being "upper field first" and NTSC being "lower field first". It is as if the capture board never switches to NTSC field order.
We have tried two different NTSC video sources, one of which was a camcorder.
However there is no field order problem with PAL signals.
We believe there is something missing from the e-consystems drivers that tells the capture board to interpret the fields correctly. We have looked in the i.MX53 Reference Manual but haven't found what hardware interface controls this.
解決済! 解決策の投稿を見る。
The NTSC field flip problem is solved.
I have found a bug in ipu_param_mem.h, the macro ipu_ch_param_mod_field can't handle negative signed values properly, as required to set a negative interlace offset (ILO). Same would probably apply to macro ipu_ch_param_set_field
TI replied to my query on their site very promptly
http://e2e.ti.com/support/data_converters/videoconverters/f/376/p/260421/911152.aspx
Seems the problem needs to be fixed using a negative Interlace Offset.
The NTSC field flip problem is solved.
I have found a bug in ipu_param_mem.h, the macro ipu_ch_param_mod_field can't handle negative signed values properly, as required to set a negative interlace offset (ILO). Same would probably apply to macro ipu_ch_param_set_field
Hello,
Would you be able to post a patch for ipu_param_mem.h that fixes those macros? Thanks!
I haven't written a patch for the macros, instead I used an unsigned value that yielded the desired signed value.
I have solved the problem setting NTSC active_top field to 4 in mxc_v4l2_capture.c
with a value of 3 as recommended around the community (instead of the default value 13), the captured frames stop rolling but the fields are flipped.
{ | /*! NTSC */ |
.v4l2_id = V4L2_STD_NTSC,
.name = "NTSC",
.raw_width = 720, | /* SENS_FRM_WIDTH */ |
.raw_height = 525, | /* SENS_FRM_HEIGHT */ |
.active_width = 720, | /* ACT_FRM_WIDTH */ |
.active_height = 480, | /* ACT_FRM_HEIGHT */ |
.active_top = 4,
.active_left = 0,
},
I am looking into the control registers for the TVP5147M1. I have tried setting
tvp5147m1_write_reg(REG_SYNC_CONTROL, 0x10);
to change the polarity of the FID (Field ID?)
and
tvp5147m1_write_reg(REG_FID_CONTROL, 0x01 );
where I’ve defined
#define REG_FID_CONTROL (0x57)
http://pdf1.alldatasheet.com/datasheet-pdf/view/227323/TI/TVP5147M1.html
I have tried each of the above together and alone (with the other defaulted) and nothing has changed the field order problem with NTSC. I note that it looks OK when the image is slowly rolling before synchronisation, but not when it has ceased rolling.
2.11.26 Sync Control Register
Subaddress 32h
Default 00h
7 6 5 4 3 2 1 0
Reserved Polarity FID Polarity VS Polarity HS VS/VBLK HS/CS
Polarity FID: determines polarity of FID terminal
0 = First field high, second field low (default)
1 = First field low, second field high
2.11.48 Field ID Control Register
Subaddress 57h
Default 00h
7 6 5 4 3 2 1 0
656 version FID control
656 Version
0 = ITU-R BT.656-4 (default)
1 = ITU-R BT.656-3
FID control
0 = 0→1 adapts to field 1, 1→0 adapts to field 1+ field 2 (default)
1 = 0→1 adapts to field 2, 1→0 adapts to field 1+ field 2 (for TVP5147M1 EVM)