NAND Flash on iMX53

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NAND Flash on iMX53

1,318件の閲覧回数
jomeke
Contributor II

Hi guys,

is there anybody who has a desin example from a NAND flash connected to the iMX537 ?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

945件の閲覧回数
jomeke
Contributor II

Thanks for the information Florent

Florent Auger said:

Hi

 

The connection is quite straight. You can use the reference manual of the i.MX53 / table 5-3 at section 5.3.4.

You'll find there that the NAND control signals are dedicated pins with the same name.

Nevertheless, the data bus is not dedicated, and can be used on the PATA signals or EIM data signals.

 

At boot, it is important to let the processor knows where to use the data bus, and the table 7-14 at section 7.5.2.4 explains this.

 

You can check that board for a reference:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIM...

0 件の賞賛
返信

945件の閲覧回数
FlorentAuger
Contributor V

Hi

 

The connection is quite straight. You can use the reference manual of the i.MX53 / table 5-3 at section 5.3.4.

You'll find there that the NAND control signals are dedicated pins with the same name.

Nevertheless, the data bus is not dedicated, and can be used on the PATA signals or EIM data signals.

 

At boot, it is important to let the processor knows where to use the data bus, and the table 7-14 at section 7.5.2.4 explains this.

 

You can check that board for a reference:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX53SABREAUTO&fpsp=1&tab=Design_To...

0 件の賞賛
返信

945件の閲覧回数
hoanghoa
Contributor I

Hi guys,

I am porting u-boot for an mx53 board which has 512 MB Nand flash of Samsung K9F4G08.

It uses CS0 and 8 bit interface only. So which value should be for CONFIG_SYS_NAND_BASE?

The connection signal is below:

- NANDF_CS0  --> CS (to NAND chip)

- NANDF_CS1,2,3 --> not used

- PATA_DATA[0-7] --> DATA[0-7]

Expecting your help!!

HTH

0 件の賞賛
返信