Dear community,
Currently, We start designing SmartWatch use Freescale i.MX6SL solution: http://www.freescale.com/webapp/sps/site/application.jsp?code=APLSMARTWATCH
We are using Mirasol Display Module, information about feartures and timing charateristics of it assigned in the attachment.
This module used MIPI DBI Type-B Parallel Interface. We see that the Timing diagram of Mirasol Module is compatible with timing diagram of eLCDIF mode of i.MX6SL. So that I think we can use the eLCDIF mode to turn on the Mirasol module.
Am I right?
Please tell me that it can communicate with i.MX6SL or not?
Best regards.
Bay
Yes, from attached diagrams this LCD can be used with eLCDIF i.MX6SL.
You also should check LCD IO levels for compatibility with i.MX6SL.