We are attempting to recreate the Android SD card that is provided with the Sabre SDB kit. The Freescale 8GB San Disk SD card is labeled:
MX6Q-SDB
Android r13.4
110-77482 A
I am using Mfgtools-Rel-13.01.00_ER_MX6Q_UPDATER that comes with the latest JB4.2.2.1.1.0 download.
I have the following setting in my INI file:
[profiles]
chip = MX6Q Linux Update
[platform]
board = SabreSD
[LIST]
name = Android-SabreSD-SD
After running Mgftool2, I noticed that the number of partitions on the new SD card does not match the Freescale Android SD card.
已解决! 转到解答。
Not sure if this is the answer but you are comparing different Android versions (ICS versus JB) , which may (I am not Android expert) have different # of partitions.
Leo