Hello community,
Can SAI's TX be set to a maximum of only 9 outputs?
In IMX8M Nano, it have 5x SAI module and Tx/Rx are following.
Five external SAI (synchronous audio interface) modules supporting I2S, AC97,
TDM, codec/DSP and DSD interfaces, including one SAI with 4 TX and 4 RX lanes,
two SAI with 2 TX and 2 RX lanes, and two SAI with 1 TX and 1 RX lanes.
It seems that total TX lanes are 10.( 4x1 + 2x2 + 1x2)
But SAI2_TXD0 and SAI5_TXD3 can allocate only same output pin.
Can SAI's TX be set to a maximum of only 9 outputs?
Best regards,
Ishii.
解決済! 解決策の投稿を見る。
Hi @takayuki_ishii,
Hope you are doing well.
Pin No. AC22 can be configured either as SAI2_TXD0 or SAI5_TX_DATA3. So, maximum 9 output data channels can be used for SAI TX.
Thanks & Regards,
Ritesh M Patel
Hi @takayuki_ishii,
Hope you are doing well.
Pin No. AC22 can be configured either as SAI2_TXD0 or SAI5_TX_DATA3. So, maximum 9 output data channels can be used for SAI TX.
Thanks & Regards,
Ritesh M Patel