MX8-DSI-OLED1 display issue with i.MX 8M Mini EVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MX8-DSI-OLED1 display issue with i.MX 8M Mini EVK

1,321 Views
frk
Contributor III

Hi,

I'm evaluating the last version of Yocto for the i.MX 8M Mini EVK with QT6 and I would to use our MX8-DSI-OLED1 screen.

Regarding the screen quick start documentation, i've got to set fdt_file in uboot with the right .dtb name.

 

The problem is that the screen doesn't show anything.

The hardware is working because with a 2019 BSP, I've got Weston that show up on the screen.

 

My boot log is the following :

 

root@imx8mm-lpddr4-evk:~# find / -name "*.dtb"
/run/media/mmcblk1p1/imx8mm-evk-8mic-revE.dtb
/run/media/mmcblk1p1/imx8mm-evk-8mic-swpdm.dtb
/run/media/mmcblk1p1/imx8mm-evk-ak4497.dtb
/run/media/mmcblk1p1/imx8mm-evk-ak5558.dtb
/run/media/mmcblk1p1/imx8mm-evk-audio-tdm.dtb
/run/media/mmcblk1p1/imx8mm-evk-dpdk.dtb
/run/media/mmcblk1p1/imx8mm-evk-ecspi-slave.dtb
/run/media/mmcblk1p1/imx8mm-evk-inmate.dtb
/run/media/mmcblk1p1/imx8mm-evk-lk.dtb
/run/media/mmcblk1p1/imx8mm-evk-pcie-ep.dtb
/run/media/mmcblk1p1/imx8mm-evk-qca-wifi.dtb
/run/media/mmcblk1p1/imx8mm-evk-revb-qca-wifi.dtb
/run/media/mmcblk1p1/imx8mm-evk-rm67191-cmd-ram.dtb
/run/media/mmcblk1p1/imx8mm-evk-rm67191.dtb
/run/media/mmcblk1p1/imx8mm-evk-rm67199-cmd-ram.dtb
/run/media/mmcblk1p1/imx8mm-evk-rm67199.dtb
/run/media/mmcblk1p1/imx8mm-evk-root.dtb
/run/media/mmcblk1p1/imx8mm-evk-rpmsg-wm8524.dtb
/run/media/mmcblk1p1/imx8mm-evk-rpmsg.dtb
/run/media/mmcblk1p1/imx8mm-evk-usd-wifi.dtb
/run/media/mmcblk1p1/imx8mm-evk.dtb
root@imx8mm-lpddr4-evk:~#
U-Boot SPL 2021.04-lf_v2021.04+gf7b43f8b4c (Mar 01 2022 - 07:31:56 +0000)
Can't find PMIC:PCA9450
DDRINFO: start DRAM init
DDRINFO: DRAM rate 3000MTS
DDRINFO:ddrphy calibration done
DDRINFO: ddrmix config done
SEC0: RNG instantiated
Normal Boot
Trying to boot from MMC1
NOTICE: BL31: v2.4(release):lf-5.15.5-1.0.0-0-g05f788b9b
NOTICE: BL31: Built : 05:49:10, Mar 2 2022


U-Boot 2021.04-lf_v2021.04+gf7b43f8b4c (Mar 01 2022 - 07:31:56 +0000)

CPU: i.MX8MMQ rev1.0 1800 MHz (running at 1200 MHz)
CPU: Commercial temperature grade (0C to 95C) at 42C
Reset cause: POR
Model: NXP i.MX8MM EVK board
DRAM: 2 GiB
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x52]
Power supply on USB2
TCPC: Vendor ID [0x1fc9], Product ID [0x5110], Addr [I2C1 0x50]
MMC: FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... *** Warning - bad CRC, using default environment

[*]-Video Link 0adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
mxs_video lcdif@32e00000: failed to get any video link display timings
probe video device failed, ret -22

[0] lcdif@32e00000, video
[1] mipi_dsi@32e10000, video_bridge
[2] adv7535@3d, panel
adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
mxs_video lcdif@32e00000: failed to get any video link display timings
probe video device failed, ret -22
In: serial
Out: serial
Err: serial
SEC0: RNG instantiated

BuildInfo:
- ATF 05f788b

switch to partitions #0, OK
mmc1 is current device
flash target is MMC:1
Net: eth0: ethernet@30be0000
Fastboot: Normal
Normal Boot
Hit any key to stop autoboot: 0
u-boot=> setenv fdt_file imx8mm-evk-rm67191.dtb
u-boot=> run bootcmd
starting USB...
Bus usb@32e40000: Port not available.
USB is stopped. Please issue 'usb start' first.
switch to partitions #0, OK
mmc1 is current device
Scanning mmc 1:1...
48127 bytes read in 3 ms (15.3 MiB/s)
Scanning disk mmc@30b50000.blk...
Scanning disk mmc@30b60000.blk...
** Unrecognized filesystem type **
** Unrecognized filesystem type **
** Unrecognized filesystem type **
** Unrecognized filesystem type **
** Unrecognized filesystem type **
** Unrecognized filesystem type **
** Unrecognized filesystem type **
** Unrecognized filesystem type **
** Unrecognized filesystem type **
** Unrecognized filesystem type **
Found 19 disks
No EFI system partition
adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
mxs_video lcdif@32e00000: failed to get any video link display timings
BootOrder not defined
EFI boot manager: Cannot load any image
switch to partitions #0, OK
mmc2(part 0) is current device
** Unrecognized filesystem type **
Running BSP bootcmd ...
switch to partitions #0, OK
mmc1 is current device
Failed to load 'boot.scr'
30792192 bytes read in 331 ms (88.7 MiB/s)
Booting from mmc ...
48127 bytes read in 3 ms (15.3 MiB/s)
Moving Image from 0x40480000 to 0x40600000, end=423f0000
## Flattened Device Tree blob at 43000000
Booting using the fdt blob at 0x43000000
Using Device Tree in place at 0000000043000000, end 000000004300ebfe
adv7535_mipi2hdmi adv7535@3d: Can't find cec device id=0x3c
fail to probe panel device adv7535@3d
mxs_video lcdif@32e00000: failed to get any video link display timings
probe video device failed, ret -22

Starting kernel ...

[ 0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[ 0.000000] Linux version 5.15.5-lts-next+gc1084c2773fc (oe-user@oe-host) (aarch64-poky-linux-gcc (GCC) 11.2.0, GNU ld (GNU Binutils) 2.37.20210721) #1 SMP PREEMPT Mon Mar 7 20:03:59 UTC 2022
[ 0.000000] Machine model: FSL i.MX8MM EVK board
[ 0.000000] efi: UEFI not found.
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000096000000, size 640 MiB
[ 0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] NUMA: No NUMA configuration found
[ 0.000000] NUMA: Faking a node at [mem 0x0000000040000000-0x00000000bdffffff]
[ 0.000000] NUMA: NODE_DATA [mem 0x95bd0800-0x95bd2fff]
[ 0.000000] Zone ranges:
[ 0.000000] DMA [mem 0x0000000040000000-0x00000000bdffffff]
[ 0.000000] DMA32 empty
[ 0.000000] Normal empty
[ 0.000000] Movable zone start for each node
[ 0.000000] Early memory node ranges
[ 0.000000] node 0: [mem 0x0000000040000000-0x00000000bdffffff]
[ 0.000000] Initmem setup node 0 [mem 0x0000000040000000-0x00000000bdffffff]
[ 0.000000] psci: probing for conduit method from DT.
[ 0.000000] psci: PSCIv1.1 detected in firmware.
[ 0.000000] psci: Using standard PSCI v0.2 function IDs
[ 0.000000] psci: Trusted OS migration not required
[ 0.000000] psci: SMC Calling Convention v1.2
[ 0.000000] percpu: Embedded 20 pages/cpu s41048 r8192 d32680 u81920
[ 0.000000] Detected VIPT I-cache on CPU0
[ 0.000000] CPU features: detected: GIC system register CPU interface
[ 0.000000] CPU features: detected: ARM erratum 845719
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 508032
[ 0.000000] Policy zone: DMA
[ 0.000000] Kernel command line: console=ttymxc1,115200 root=/dev/mmcblk1p2 rootwait rw
[ 0.000000] Dentry cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[ 0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[ 0.000000] Memory: 1337876K/2064384K available (18432K kernel code, 1526K rwdata, 7032K rodata, 2944K init, 535K bss, 71148K reserved, 655360K cma-reserved)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] rcu: Preemptible hierarchical RCU implementation.
[ 0.000000] rcu: RCU event tracing is enabled.
[ 0.000000] rcu: RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
[ 0.000000] Trampoline variant of Tasks RCU enabled.
[ 0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[ 0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
[ 0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[ 0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[ 0.000000] GICv3: 128 SPIs implemented
[ 0.000000] GICv3: 0 Extended SPIs implemented
[ 0.000000] GICv3: Distributor has no Range Selector support
[ 0.000000] Root IRQ handler: gic_handle_irq
[ 0.000000] GICv3: 16 PPIs implemented
[ 0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000038880000
[ 0.000000] ITS: No ITS available, not enabling LPIs
[ 0.000000] random: get_random_bytes called from start_kernel+0x474/0x660 with crng_init=0
[ 0.000000] arch_timer: cp15 timer(s) running at 8.00MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x1d854df40, max_idle_ns: 440795202120 ns
[ 0.000000] sched_clock: 56 bits at 8MHz, resolution 125ns, wraps every 2199023255500ns
[ 0.000385] Console: colour dummy device 80x25
[ 0.000459] Calibrating delay loop (skipped), value calculated using timer frequency.. 16.00 BogoMIPS (lpj=32000)
[ 0.000473] pid_max: default: 32768 minimum: 301
[ 0.000532] LSM: Security Framework initializing
[ 0.000591] Mount-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.000605] Mountpoint-cache hash table entries: 4096 (order: 3, 32768 bytes, linear)
[ 0.001869] rcu: Hierarchical SRCU implementation.
[ 0.002841] EFI services will not be available.
[ 0.003020] smp: Bringing up secondary CPUs ...
[ 0.003401] Detected VIPT I-cache on CPU1
[ 0.003429] GICv3: CPU1: found redistributor 1 region 0:0x00000000388a0000
[ 0.003477] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[ 0.003901] Detected VIPT I-cache on CPU2
[ 0.003922] GICv3: CPU2: found redistributor 2 region 0:0x00000000388c0000
[ 0.003950] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
[ 0.004344] Detected VIPT I-cache on CPU3
[ 0.004361] GICv3: CPU3: found redistributor 3 region 0:0x00000000388e0000
[ 0.004387] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
[ 0.004444] smp: Brought up 1 node, 4 CPUs
[ 0.004461] SMP: Total of 4 processors activated.
[ 0.004467] CPU features: detected: 32-bit EL0 Support
[ 0.004471] CPU features: detected: 32-bit EL1 Support
[ 0.004481] CPU features: detected: CRC32 instructions
[ 0.012193] CPU: All CPU(s) started at EL2
[ 0.012220] alternatives: patching kernel code
[ 0.013577] devtmpfs: initialized
[ 0.020156] KASLR disabled due to lack of seed
[ 0.020302] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[ 0.020323] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[ 0.043354] pinctrl core: initialized pinctrl subsystem
[ 0.043906] DMI not present or invalid.
[ 0.044351] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[ 0.049350] DMA: preallocated 256 KiB GFP_KERNEL pool for atomic allocations
[ 0.049753] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[ 0.050124] DMA: preallocated 256 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[ 0.050230] audit: initializing netlink subsys (disabled)
[ 0.050522] audit: type=2000 audit(0.048:1): state=initialized audit_enabled=0 res=1
[ 0.051082] thermal_sys: Registered thermal governor 'step_wise'
[ 0.051088] thermal_sys: Registered thermal governor 'power_allocator'
[ 0.051284] cpuidle: using governor menu
[ 0.051491] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[ 0.051589] ASID allocator initialised with 65536 entries
[ 0.052453] Serial: AMBA PL011 UART driver
[ 0.052514] imx mu driver is registered.
[ 0.052535] imx rpmsg driver is registered.
[ 0.063694] imx8mm-pinctrl 30330000.pinctrl: initialized IMX pinctrl driver
[ 0.073335] platform 32e10000.mipi_dsi: Fixing up cyclic dependency with 32e00000.lcdif
[ 0.073995] platform 32e30000.mipi_csi: Fixing up cyclic dependency with 32e20000.csi1_bridge
[ 0.095499] HugeTLB registered 1.00 GiB page size, pre-allocated 0 pages
[ 0.095520] HugeTLB registered 32.0 MiB page size, pre-allocated 0 pages
[ 0.095529] HugeTLB registered 2.00 MiB page size, pre-allocated 0 pages
[ 0.095537] HugeTLB registered 64.0 KiB page size, pre-allocated 0 pages
[ 0.096614] cryptd: max_cpu_qlen set to 1000
[ 0.099419] ACPI: Interpreter disabled.
[ 0.100140] iommu: Default domain type: Translated
[ 0.100150] iommu: DMA domain TLB invalidation policy: strict mode
[ 0.100318] vgaarb: loaded
[ 0.100601] SCSI subsystem initialized
[ 0.100908] usbcore: registered new interface driver usbfs
[ 0.100944] usbcore: registered new interface driver hub
[ 0.100973] usbcore: registered new device driver usb
[ 0.101844] mc: Linux media interface: v0.10
[ 0.101870] videodev: Linux video capture interface: v2.00
[ 0.101941] pps_core: LinuxPPS API ver. 1 registered
[ 0.101947] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.101961] PTP clock support registered
[ 0.102118] EDAC MC: Ver: 3.0.0
[ 0.103173] FPGA manager framework
[ 0.103248] Advanced Linux Sound Architecture Driver Initialized.
[ 0.103767] Bluetooth: Core ver 2.22
[ 0.103797] NET: Registered PF_BLUETOOTH protocol family
[ 0.103804] Bluetooth: HCI device and connection manager initialized
[ 0.103815] Bluetooth: HCI socket layer initialized
[ 0.103823] Bluetooth: L2CAP socket layer initialized
[ 0.103837] Bluetooth: SCO socket layer initialized
[ 0.104523] clocksource: Switched to clocksource arch_sys_counter
[ 0.104667] VFS: Disk quotas dquot_6.6.0
[ 0.104711] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[ 0.104861] pnp: PnP ACPI: disabled
[ 0.110833] NET: Registered PF_INET protocol family
[ 0.110963] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[ 0.111880] tcp_listen_portaddr_hash hash table entries: 1024 (order: 2, 16384 bytes, linear)
[ 0.111914] TCP established hash table entries: 16384 (order: 5, 131072 bytes, linear)
[ 0.112053] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, linear)
[ 0.112289] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.112380] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.112426] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[ 0.112592] NET: Registered PF_UNIX/PF_LOCAL protocol family
[ 0.112947] RPC: Registered named UNIX socket transport module.
[ 0.112955] RPC: Registered udp transport module.
[ 0.112961] RPC: Registered tcp transport module.
[ 0.112968] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.113672] PCI: CLS 0 bytes, default 64
[ 0.114210] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[ 0.114988] kvm [1]: IPA Size Limit: 40 bits
[ 0.116500] kvm [1]: GICv3: no GICV resource entry
[ 0.116508] kvm [1]: disabling GICv2 emulation
[ 0.116549] kvm [1]: GIC system register CPU interface enabled
[ 0.116622] kvm [1]: vgic interrupt IRQ9
[ 0.116736] kvm [1]: Hyp mode initialized successfully
[ 0.119757] Initialise system trusted keyrings
[ 0.119885] workingset: timestamp_bits=42 max_order=19 bucket_order=0
[ 0.125800] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.126384] NFS: Registering the id_resolver key type
[ 0.126409] Key type id_resolver registered
[ 0.126417] Key type id_legacy registered
[ 0.126488] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[ 0.126496] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[ 0.126517] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 0.126851] 9p: Installing v9fs 9p2000 file system support
[ 0.163047] Key type asymmetric registered
[ 0.163056] Asymmetric key parser 'x509' registered
[ 0.163121] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 243)
[ 0.163129] io scheduler mq-deadline registered
[ 0.163136] io scheduler kyber registered
[ 0.169347] EINJ: ACPI disabled.
[ 0.178983] imx-sdma 302c0000.dma-controller: Direct firmware load for imx/sdma/sdma-imx7d.bin failed with error -2
[ 0.179008] imx-sdma 302c0000.dma-controller: Falling back to sysfs fallback for: imx/sdma/sdma-imx7d.bin
[ 0.185559] mxs-dma 33000000.dma-controller: initialized
[ 0.187086] SoC: i.MX8MM revision 1.0
[ 0.187538] Bus freq driver module loaded
[ 0.193081] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.195421] 30860000.serial: ttymxc0 at MMIO 0x30860000 (irq = 47, base_baud = 5000000) is a IMX
[ 0.195948] 30880000.serial: ttymxc2 at MMIO 0x30880000 (irq = 48, base_baud = 5000000) is a IMX
[ 0.196374] 30890000.serial: ttymxc1 at MMIO 0x30890000 (irq = 49, base_baud = 1500000) is a IMX
[ 1.227007] printk: console [ttymxc1] enabled
[ 1.246755] loop: module loaded
[ 1.251205] of_reserved_mem_lookup() returned NULL
[ 1.256079] megasas: 07.717.02.00-rc1
[ 1.261334] imx ahci driver is registered.
[ 1.266319] SPI driver mtd_dataflash has no spi_device_id for atmel,at45
[ 1.273033] SPI driver mtd_dataflash has no spi_device_id for atmel,dataflash
[ 1.282971] spi-nor spi0.0: n25q256ax1 (32768 Kbytes)
[ 1.294703] libphy: Fixed MDIO Bus: probed
[ 1.300267] tun: Universal TUN/TAP device driver, 1.6
[ 1.306168] thunder_xcv, ver 1.0
[ 1.309440] thunder_bgx, ver 1.0
[ 1.312703] nicpf, ver 1.0
[ 1.317510] hclge is initializing
[ 1.320855] hns3: Hisilicon Ethernet Network Driver for Hip08 Family - version
[ 1.328085] hns3: Copyright (c) 2017 Huawei Corporation.
[ 1.333449] e1000: Intel(R) PRO/1000 Network Driver
[ 1.338335] e1000: Copyright (c) 1999-2006 Intel Corporation.
[ 1.344122] e1000e: Intel(R) PRO/1000 Network Driver
[ 1.349091] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[ 1.355100] igb: Intel(R) Gigabit Ethernet Network Driver
[ 1.360517] igb: Copyright (c) 2007-2014 Intel Corporation.
[ 1.366129] igbvf: Intel(R) Gigabit Virtual Function Network Driver
[ 1.372404] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
[ 1.378512] sky2: driver version 1.30
[ 1.382762] usbcore: registered new interface driver r8152
[ 1.388504] VFIO - User Level meta-driver version: 0.3
[ 1.395958] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 1.402511] ehci-pci: EHCI PCI platform driver
[ 1.406998] ehci-platform: EHCI generic platform driver
[ 1.412434] ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver
[ 1.418661] ohci-pci: OHCI PCI platform driver
[ 1.423142] ohci-platform: OHCI generic platform driver
[ 1.429133] usbcore: registered new interface driver uas
[ 1.434500] usbcore: registered new interface driver usb-storage
[ 1.440577] usbcore: registered new interface driver usbserial_generic
[ 1.447130] usbserial: USB Serial support registered for generic
[ 1.453165] usbcore: registered new interface driver ftdi_sio
[ 1.458935] usbserial: USB Serial support registered for FTDI USB Serial Device
[ 1.466276] usbcore: registered new interface driver usb_serial_simple
[ 1.472826] usbserial: USB Serial support registered for carelink
[ 1.478945] usbserial: USB Serial support registered for zio
[ 1.484626] usbserial: USB Serial support registered for funsoft
[ 1.490652] usbserial: USB Serial support registered for flashloader
[ 1.497027] usbserial: USB Serial support registered for google
[ 1.502972] usbserial: USB Serial support registered for libtransistor
[ 1.509518] usbserial: USB Serial support registered for vivopay
[ 1.515544] usbserial: USB Serial support registered for moto_modem
[ 1.521835] usbserial: USB Serial support registered for motorola_tetra
[ 1.528468] usbserial: USB Serial support registered for novatel_gps
[ 1.534841] usbserial: USB Serial support registered for hp4x
[ 1.540608] usbserial: USB Serial support registered for suunto
[ 1.546547] usbserial: USB Serial support registered for siemens_mpi
[ 1.552937] usbcore: registered new interface driver usb_ehset_test
[ 1.562205] input: 30370000.snvs:snvs-powerkey as /devices/platform/soc@0/30000000.bus/30370000.snvs/30370000.snvs:snvs-powerkey/input/input0
[ 1.576600] snvs_rtc 30370000.snvs:snvs-rtc-lp: registered as rtc0
[ 1.582813] snvs_rtc 30370000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01T00:01:25 UTC (85)
[ 1.592078] i2c_dev: i2c /dev entries driver
[ 1.597365] mx6s-csi 32e20000.csi1_bridge: initialising
[ 1.606187] Bluetooth: HCI UART driver ver 2.3
[ 1.610667] Bluetooth: HCI UART protocol H4 registered
[ 1.615814] Bluetooth: HCI UART protocol BCSP registered
[ 1.621157] Bluetooth: HCI UART protocol LL registered
[ 1.626301] Bluetooth: HCI UART protocol ATH3K registered
[ 1.631720] Bluetooth: HCI UART protocol Three-wire (H5) registered
[ 1.638084] Bluetooth: HCI UART protocol Broadcom registered
[ 1.643773] Bluetooth: HCI UART protocol QCA registered
[ 1.650557] sdhci: Secure Digital Host Controller Interface driver
[ 1.656765] sdhci: Copyright(c) Pierre Ossman
[ 1.661787] SPI driver mmc_spi has no spi_device_id for mmc-spi-slot
[ 1.668174] Synopsys Designware Multimedia Card Interface Driver
[ 1.674840] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.682712] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.689785] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
[ 1.696731] usbcore: registered new interface driver usbhid
[ 1.702313] usbhid: USB HID core driver
[ 1.710115] cs_system_cfg: CoreSight Configuration manager initialised
[ 1.713931] mmc2: SDHCI controller on 30b60000.mmc [30b60000.mmc] using ADMA
[ 1.718270] optee: probing for conduit method.
[ 1.728297] optee: revision 3.15 (807629a0)
[ 1.729487] optee: dynamic shared memory is enabled
[ 1.738919] optee: initialized driver
[ 1.744171] galcore: clk_get vg clock failed, disable vg!
[ 1.750033] Galcore version 6.4.3.p4.398061
[ 1.805015] mmc2: new HS400 Enhanced strobe MMC card at address 0001
[ 1.812314] mmcblk2: mmc2:0001 DG4016 14.7 GiB
[ 1.813272] [drm] Initialized vivante 1.0.0 20170808 for 38000000.gpu on minor 0
[ 1.821207] Alternate GPT is invalid, using primary GPT.
[ 1.826011] hantrodec 0 : module inserted. Major = 511
[ 1.829646] mmcblk2: p1 p2 p3 p4 p5 p6 p7 p8 p9 p10 p11 p12 p13 p14 p15
[ 1.835251] hantrodec 1 : module inserted. Major = 511
[ 1.847534] hx280enc: module inserted. Major <510>
[ 1.849066] mmcblk2boot0: mmc2:0001 DG4016 4.00 MiB
[ 1.857931] NET: Registered PF_LLC protocol family
[ 1.858523] mmcblk2boot1: mmc2:0001 DG4016 4.00 MiB
[ 1.863258] NET: Registered PF_INET6 protocol family
[ 1.868789] mmcblk2rpmb: mmc2:0001 DG4016 4.00 MiB, chardev (234:0)
[ 1.874810] Segment Routing with IPv6
[ 1.882675] In-situ OAM (IOAM) with IPv6
[ 1.886648] NET: Registered PF_PACKET protocol family
[ 1.892438] Bluetooth: RFCOMM TTY layer initialized
[ 1.897337] Bluetooth: RFCOMM socket layer initialized
[ 1.902497] Bluetooth: RFCOMM ver 1.11
[ 1.906261] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 1.911578] Bluetooth: BNEP filters: protocol multicast
[ 1.916813] Bluetooth: BNEP socket layer initialized
[ 1.921783] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 1.927710] Bluetooth: HIDP socket layer initialized
[ 1.933724] 8021q: 802.1Q VLAN Support v1.8
[ 1.937938] lib80211: common routines for IEEE802.11 drivers
[ 1.943712] 9pnet: Installing 9P2000 support
[ 1.948019] tsn generic netlink module v1 init...
[ 1.952806] Key type dns_resolver registered
[ 1.957992] Loading compiled-in X.509 certificates
[ 1.987029] usb_phy_generic usbphynop1: supply vcc not found, using dummy regulator
[ 1.994964] usb_phy_generic usbphynop2: supply vcc not found, using dummy regulator
[ 2.004245] nxp-pca9450 0-0025: Read device id error
[ 2.009419] i2c i2c-0: IMX I2C adapter registered
[ 2.015252] i2c 1-003d: Fixing up cyclic dependency with 32e10000.mipi_dsi
[ 2.022459] adv7511 1-003d: supply avdd not found, using dummy regulator
[ 2.029287] adv7511 1-003d: supply dvdd not found, using dummy regulator
[ 2.036031] adv7511 1-003d: supply pvdd not found, using dummy regulator
[ 2.042775] adv7511 1-003d: supply a2vdd not found, using dummy regulator
[ 2.049604] adv7511 1-003d: supply v3p3 not found, using dummy regulator
[ 2.056342] adv7511 1-003d: supply v1p2 not found, using dummy regulator
[ 2.063887] adv7511 1-003d: Probe failed. Remote port 'mipi_dsi@32e10000' disabled
[ 2.071722] i2c 1-0050: Fixing up cyclic dependency with 32e40000.usb
[ 2.080174] i2c i2c-1: IMX I2C adapter registered
[ 2.087293] i2c 2-003c: Fixing up cyclic dependency with 32e30000.mipi_csi
[ 2.094629] ov5640_mipi 2-003c: No sensor reset pin available
[ 2.100413] ov5640_mipi 2-003c: supply DOVDD not found, using dummy regulator
[ 2.107667] ov5640_mipi 2-003c: supply DVDD not found, using dummy regulator
[ 2.114761] ov5640_mipi 2-003c: supply AVDD not found, using dummy regulator
[ 2.136828] ov5640_mipi 2-003c: Read reg error: reg=300a
[ 2.142158] ov5640_mipi 2-003c: Camera is not found
[ 2.147339] i2c i2c-2: IMX I2C adapter registered
[ 2.154492] imx6q-pcie 33800000.pcie: supply epdev_on not found, using dummy regulator
[ 2.157397] imx-drm 32c00000.bus:display-subsystem: bound imx-lcdif-crtc.0 (ops lcdif_crtc_ops)
[ 2.162794] imx6q-pcie 33800000.pcie: EXT REF_CLK is used!.
[ 2.171330] imx_sec_dsim_drv 32e10000.mipi_dsi: version number is 0x1060200
[ 2.183744] [drm:drm_bridge_attach] *ERROR* failed to attach bridge /soc@0/bus@32c00000/mipi_dsi@32e10000 to encoder DSI-34: -19
[ 2.195347] imx_sec_dsim_drv 32e10000.mipi_dsi: Failed to attach bridge: 32e10000.mipi_dsi
[ 2.203623] imx_sec_dsim_drv 32e10000.mipi_dsi: failed to bind sec dsim bridge: -19
[ 2.204894] imx6q-pcie 33800000.pcie: PCIe PLL is locked.
[ 2.211290] imx-drm 32c00000.bus:display-subsystem: bound 32e10000.mipi_dsi (ops imx_sec_dsim_ops)
[ 2.216737] imx6q-pcie 33800000.pcie: invalid resource
[ 2.226030] [drm] Initialized imx-drm 1.0.0 20120507 for 32c00000.bus:display-subsystem on minor 1
[ 2.230798] imx6q-pcie 33800000.pcie: iATU unroll: enabled
[ 2.243891] pps pps0: new PPS source ptp0
[ 2.245257] imx6q-pcie 33800000.pcie: Detected iATU regions: 4 outbound, 4 inbound
[ 2.245269] imx6q-pcie 33800000.pcie: host bridge /soc@0/pcie@33800000 ranges:
[ 2.264173] imx6q-pcie 33800000.pcie: IO 0x001ff80000..0x001ff8ffff -> 0x0000000000
[ 2.272401] imx6q-pcie 33800000.pcie: MEM 0x0018000000..0x001fefffff -> 0x0018000000
[ 2.280757] imx6q-pcie 33800000.pcie: iATU unroll: enabled
[ 2.286324] imx6q-pcie 33800000.pcie: Detected iATU regions: 4 outbound, 4 inbound
[ 2.296679] libphy: fec_enet_mii_bus: probed
[ 2.303968] fec 30be0000.ethernet eth0: registered PHC device 0
[ 2.316079] mxc_mipi-csi 32e30000.mipi_csi: supply mipi-phy not found, using dummy regulator
[ 2.324908] mxc_mipi-csi 32e30000.mipi_csi: mipi csi v4l2 device registered
[ 2.331894] CSI: Registered sensor subdevice: mxc_mipi-csi.0
[ 2.337578] mxc_mipi-csi 32e30000.mipi_csi: lanes: 2, hs_settle: 13, clk_settle: 2, wclk: 1, freq: 333000000
[ 2.347939] imx-cpufreq-dt imx-cpufreq-dt: cpu speed grade 3 mkt segment 0 supported-hw 0x8 0x1
[ 2.359966] sdhci-esdhc-imx 30b50000.mmc: Got CD GPIO
[ 2.361392] sdhci-esdhc-imx 30b40000.mmc: allocated mmc-pwrseq
[ 2.372710] OF: graph: no port node found in /soc@0/bus@30800000/i2c@30a30000/tcpc@50/connector
[ 2.381504] OF: graph: no port node found in /soc@0/bus@30800000/i2c@30a30000/tcpc@50/connector
[ 2.399539] mmc1: SDHCI controller on 30b50000.mmc [30b50000.mmc] using ADMA
[ 2.402628] mmc0: SDHCI controller on 30b40000.mmc [30b40000.mmc] using ADMA
[ 2.421865] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[ 2.430893] random: fast init done
[ 2.436222] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[ 2.444631] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[ 2.449109] ALSA device list:
[ 2.453314] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[ 2.456227] No soundcards found.
[ 2.473940] mmc0: queuing unknown CIS tuple 0x01 [d9 01 ff] (3 bytes)
[ 2.488182] mmc0: queuing unknown CIS tuple 0x1a [01 01 00 02 07] (5 bytes)
[ 2.498556] mmc0: queuing unknown CIS tuple 0x1b [c1 41 30 30 ff ff 32 00] (8 bytes)
[ 2.506991] mmc0: queuing unknown CIS tuple 0x14 [] (0 bytes)
[ 2.527741] mmc0: new ultra high speed SDR104 SDIO card at address 0001
[ 2.586930] mmc1: host does not support reading read-only switch, assuming write-enable
[ 2.625848] mmc1: new ultra high speed SDR104 SDHC card at address e624
[ 2.633602] mmcblk1: mmc1:e624 SC16G 14.8 GiB
[ 2.645195] mmcblk1: p1 p2
[ 3.291859] imx6q-pcie 33800000.pcie: Phy link never came up
[ 3.297641] imx6q-pcie: probe of 33800000.pcie failed with error -110
[ 3.327505] EXT4-fs (mmcblk1p2): recovery complete
[ 3.334021] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Opts: (null). Quota mode: none.
[ 3.343839] VFS: Mounted root (ext4 filesystem) on device 179:98.
[ 3.354107] devtmpfs: mounted
[ 3.357826] Freeing unused kernel memory: 2944K
[ 3.362460] Run /sbin/init as init process
[ 3.532509] systemd[1]: System time before build time, advancing clock.
[ 3.555856] systemd[1]: systemd 249 running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid)
[ 3.589897] systemd[1]: Detected architecture arm64.

Welcome to NXP i.MX Release Distro 5.15-honister (honister)!

[ 3.636457] systemd[1]: Hostname set to <imx8mm-lpddr4-evk>.
[ 3.706570] systemd-sysv-generator[190]: SysV service '/etc/init.d/rc.local' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.731593] systemd-sysv-generator[190]: SysV service '/etc/init.d/save-rtc.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.756449] systemd-sysv-generator[190]: SysV service '/etc/init.d/umountfs' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.781392] systemd-sysv-generator[190]: SysV service '/etc/init.d/umountnfs.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.805753] systemd-sysv-generator[190]: SysV service '/etc/init.d/single' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.833435] systemd-sysv-generator[190]: SysV service '/etc/init.d/reboot' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.861075] systemd-sysv-generator[190]: SysV service '/etc/init.d/sendsigs' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 3.885330] systemd-sysv-generator[190]: SysV service '/etc/init.d/halt' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[ 4.262014] systemd[1]: Queued start job for default target Graphical Interface.
[ 4.270676] random: systemd: uninitialized urandom read (16 bytes read)
[ 4.334100] systemd[1]: Created slice Slice /system/getty.
[ OK ] Created slice Slice /system/getty.
[ 4.346865] random: systemd: uninitialized urandom read (16 bytes read)
[ 4.356046] systemd[1]: Created slice Slice /system/modprobe.
[ OK ] Created slice Slice /system/modprobe.
[ 4.376742] random: systemd: uninitialized urandom read (16 bytes read)
[ 4.385982] systemd[1]: Created slice Slice /system/serial-getty.
[ OK ] Created slice Slice /system/serial-getty.
[ 4.411211] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 4.432997] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password …ts to Console Directory Watch.
[ 4.457261] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ OK ] Started Forward Password R…uests to Wall Directory Watch.
[ 4.480901] systemd[1]: Reached target Host and Network Name Lookups.
[ OK ] Reached target Host and Network Name Lookups.
[ 4.505058] systemd[1]: Reached target Path Units.
[ OK ] Reached target Path Units.
[ 4.525067] systemd[1]: Reached target Remote File Systems.
[ OK ] Reached target Remote File Systems.
[ 4.549043] systemd[1]: Reached target Slice Units.
[ OK ] Reached target Slice Units.
[ 4.569076] systemd[1]: Reached target Swaps.
[ OK ] Reached target Swaps.
[ 4.596542] systemd[1]: Listening on RPCbind Server Activation Socket.
[ OK ] Listening on RPCbind Server Activation Socket.
[ 4.621130] systemd[1]: Reached target RPC Port Mapper.
[ OK ] Reached target RPC Port Mapper.
[ 4.641469] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 4.661298] systemd[1]: Listening on initctl Compatibility Named Pipe.
[ OK ] Listening on initctl Compatibility Named Pipe.
[ 4.685726] systemd[1]: Listening on Journal Audit Socket.
[ OK ] Listening on Journal Audit Socket.
[ 4.698584] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 4.721564] systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
[ 4.741415] systemd[1]: Listening on Network Service Netlink Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ 4.769444] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 4.782343] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 4.805509] systemd[1]: Listening on User Database Manager Socket.
[ OK ] Listening on User Database Manager Socket.
[ 4.833126] systemd[1]: Mounting Huge Pages File System...
Mounting Huge Pages File System...
[ 4.856702] systemd[1]: Mounting POSIX Message Queue File System...
Mounting POSIX Message Queue File System...
[ 4.884713] systemd[1]: Mounting Kernel Debug File System...
Mounting Kernel Debug File System...
[ 4.905071] systemd[1]: Condition check resulted in Kernel Trace File System being skipped.
[ 4.921619] systemd[1]: Mounting Temporary Directory /tmp...
Mounting Temporary Directory /tmp...
[ 4.949416] systemd[1]: Starting Create List of Static Device Nodes...
Starting Create List of Static Device Nodes...
[ 4.980923] systemd[1]: Starting Load Kernel Module configfs...
Starting Load Kernel Module configfs...
[ 5.004602] systemd[1]: Starting Load Kernel Module drm...
Starting Load Kernel Module drm...
[ 5.028482] systemd[1]: Starting Load Kernel Module fuse...
Starting Load Kernel Module fuse...
[ 5.047568] fuse: init (API version 7.34)
[ 5.072989] systemd[1]: Starting RPC Bind...
Starting RPC Bind...
[ 5.092852] systemd[1]: Condition check resulted in File System Check on Root Device being skipped.
[ 5.102891] systemd[1]: systemd-journald.service: unit configures an IP firewall, but the local system does not support BPF/cgroup firewalling.
[ 5.115895] systemd[1]: (This warning is only shown for the first unit using IP firewalling.)
[ 5.130279] systemd[1]: Starting Journal Service...
Starting Journal Service...
[ 5.156325] systemd[1]: Condition check resulted in Load Kernel Modules being skipped.
[ 5.169075] systemd[1]: Starting Remount Root and Kernel File Systems...
Starting Remount Root and Kernel File Systems...
[ 5.190936] EXT4-fs (mmcblk1p2): re-mounted. Opts: (null). Quota mode: none.
[ 5.209888] systemd[1]: Starting Apply Kernel Variables...
Starting Apply Kernel Variables...
[ 5.233398] systemd[1]: Starting Coldplug All udev Devices...
Starting Coldplug All udev Devices...
[ 5.257689] systemd[1]: Starting Setup Virtual Console...
Starting Setup Virtual Console...
[ 5.283987] systemd[1]: Started RPC Bind.
[ OK ] Started RPC Bind.
[ 5.301244] systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
[ OK ] Mounted Huge Pages File System.
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Kernel Debug File System.
[ OK ] Mounted Temporary Directory /tmp.
[ OK ] Finished Create List of Static Device Nodes.
[ OK ] Finished Load Kernel Module configfs.
[ OK ] Finished Load Kernel Module drm.
[ OK ] Finished Load Kernel Module fuse.
[ OK ] Finished Remount Root and Kernel File Systems.
[ OK ] Finished Apply Kernel Variables.
[ OK ] Finished Setup Virtual Console.
Mounting FUSE Control File System...
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
[ 5.598737] systemd-journald[200]: Received client request to flush runtime journal.
Starting Create Static Device Nodes in /dev...
[ OK ] Mounted FUSE Control File System.
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Finished Flush Journal to Persistent Storage.
[ OK ] Finished Create Static Device Nodes in /dev.
[ OK ] Reached target Preparation for Local File Systems.
Mounting /var/volatile...
Starting Rule-based Manage…for Device Events and Files...
[ OK ] Mounted /var/volatile.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Finished Coldplug All udev Devices.
[ OK ] Finished Create Volatile Files and Directories.
[ OK ] Started Rule-based Manager for Device Events and Files.
Starting Start Psplash Boot Screen...
Starting Network Time Synchronization...
Starting Record System Boot/Shutdown in UTMP...
[ OK ] Started Start Psplash Boot Screen.
[ OK ] Started Start psplash-syst…progress communication helper.
[ OK ] Finished Record System Boot/Shutdown in UTMP.
[ 6.335542] Registered IR keymap rc-empty
[ 6.340089] rc rc0: gpio_ir_recv as /devices/platform/ir-receiver/rc/rc0
[ 6.362086] input: gpio_ir_recv as /devices/platform/ir-receiver/rc/rc0/input1
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Initialization.
[ 6.415080] fsl-micfil-dai 30080000.audio-controller: GET IRQ: 24
[ 6.421652] fsl-micfil-dai 30080000.audio-controller: GET IRQ: 25
[ 6.427874] fsl-micfil-dai 30080000.audio-controller: GET IRQ: 26
[ 6.434057] fsl-micfil-dai 30080000.audio-controller: GET IRQ: 27
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target System Time Set.
[ OK ] Started Daily rotation of log files.
[ 6.487979] debugfs: File 'Playback' in directory 'dapm' already present!
[ 6.494973] debugfs: File 'Capture' in directory 'dapm' already present!
[ 6.506264] caam-snvs 30370000.caam-snvs: violation handlers armed - init state
[ OK ] Reached target Timer Units.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ 6.561584] caam 30900000.crypto: device ID = 0x0a16040100000000 (Era 9)
[ 6.570557] caam 30900000.crypto: job rings = 1, qi = 0
Starting Docker Socket for the API...
[ OK ] Listening on dropbear.socket.
Starting Weston socket...
Starting Console System Startup Logging...
[ OK ] Listening on Docker Socket for the API.
[ OK ] Listening on Weston socket.
[ OK ] Finished Console System Startup Logging.
[ OK ] Reached target Socket Units.
[ OK ] Reached target Basic System.
[ OK ] Reached target Hardware activated USB gadget.
[ OK ] Started Job spooling tools.
[ OK ] Started Periodic Command Scheduler.
[ OK ] Started D-Bus System Message Bus.
[ OK ] Started Linux Firmware Loader Daemon.
[ 6.943494] imx-sdma 302b0000.dma-controller: firmware found.
[ 6.944705] imx-sdma 302c0000.dma-controller: firmware found.
[ 6.955060] imx-sdma 302b0000.dma-controller: loaded firmware 4.6
[ 6.955730] imx-sdma 30bd0000.dma-controller: firmware found.
[ OK ] Started Configuration for i.MX GPU (Former rc_gpu.S).
Starting IPv6 Packet Filtering Framework...
Starting IPv4 Packet Filtering Framework...
Starting Network Time Service (one-shot ntpdate mode)...
Starting Telephony service...
[ OK ] Started Updates psplash to basic.
[ OK ] Started System Logging Service.
Starting User Login Management...
[ OK ] Started TEE Supplicant.
[ OK ] Finished IPv6 Packet Filtering Framework.
[ OK ] Finished IPv4 Packet Filtering Framework.
[ OK ] Finished Network Time Service (one-shot ntpdate mode).
[ OK ] Started Telephony service.
[ OK ] Reached target Preparation for Network.
Starting Connection service...
Starting Network Configuration...
[ OK ] Started Connection service.
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started User Login Management.
Starting Hostname Service...
Starting WPA supplicant...
[ OK ] Started Network Configuration.
[ OK ] Started WPA supplicant.
[ OK ] Reached target Network.
Starting containerd container runtime...
[ OK ] Started NFS status monitor for NFSv2/3 locking..
[ OK ] Started Respond to IPv6 Node Information Queries.
[ OK ] Started Update psplash to network.
Starting Terminate Psplash Boot Screen...
Starting /etc/rc.local Compatibility...
[ OK ] Started Network Router Discovery Daemon.
Starting Permit User Sessions...
[FAILED] Failed to start Terminate Psplash Boot Screen.
See 'systemctl status psplash-quit.service' for details.
[ OK ] Started /etc/rc.local Compatibility.
[ OK ] Finished Permit User Sessions.
[ 8.780609] random: crng init done
[ 8.784037] random: 7 urandom warning(s) missed due to ratelimiting
[ OK ] Finished Load/Save Random Seed.
[ OK ] Started Hostname Service.
[ 8.927991] caam algorithms registered in /proc/crypto
[ 8.935205] caam 30900000.crypto: caam pkc algorithms registered in /proc/crypto
[ 8.942950] caam 30900000.crypto: registering rng-caam
[ 8.950988] Device caam-keygen registered
[ OK ] Created slice Slice /system/systemd-fsck.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttymxc1.
[ OK ] Reached target Login Prompts.
Starting File System Check on /dev/mmcblk1p1...
Starting File System Check on /dev/mmcblk2p10...
Starting File System Check on /dev/mmcblk2p11...
Starting File System Check on /dev/mmcblk2p12...
Starting File System Check on /dev/mmcblk2p6...
Starting Weston, a Wayland…ositor, as a system service...
[ OK ] Found device /dev/mmcblk2p5.
Starting Save/Restore Sound Card State...
Starting File System Check on /dev/mmcblk2p5...
Starting User Database Manager...
[ OK ] Finished File System Check on /dev/mmcblk2p12.
Mounting /run/media/mmcblk2p12...
[ 9.248702] EXT4-fs (mmcblk2p12): The kernel was not built with CONFIG_QUOTA and CONFIG_QFMT_V2
[FAILED] Failed to mount /run/media/mmcblk2p12.
See 'systemctl status run-media-mmcblk2p12.mount' for details.
[ OK ] Finished Save/Restore Sound Card State.
[ OK ] Reached target Sound Card.
[ OK ] Finished File System Check on /dev/mmcblk1p1.
Mounting /run/media/mmcblk1p1...
[ OK ] Mounted /run/media/mmcblk1p1.
[ OK ] Started User Database Manager.
[ OK ] Created slice User Slice of UID 0.
Starting User Runtime Directory /run/user/0...
[ OK ] Finished User Runtime Directory /run/user/0.
Starting User Manager for UID 0...
[ OK ] Started containerd container runtim[ 9.641050] audit: type=1006 audit(1637342374.108:2): pid=833 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
e.
[ OK ] Reach[ 9.657172] audit: type=1300 audit(1637342374.108:2): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffc6b94ca0 a2=1 a3=ffff830cd6b0 items=0 ppid=1 pid=833 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
ed target Multi-User Sys[ 9.685364] audit: type=1327 audit(1637342374.108:2): proctitle="(systemd)"
tem.
[ OK ] Finished File System Check on /dev/mmcblk2p10.
Mounting /run/media/mmcblk2p10...
[ 9.740742] EXT4-fs (mmcblk2p10): mounted filesystem without journal. Opts: (null). Quota mode: none.
[ OK ] Finished 9.750792] ext4 filesystem being mounted at /run/media/mmcblk2p10 supports timestamps until 2038 (0x7fffffff)
1;39mFile System Check on /dev/mmcblk2p11.
Mounting /run/media/mmcblk2p11...
[ OK ] Mounted /run/media/mmcblk2p10.
[ 9.806477] EXT4-fs (mmcblk2p11): mounted filesystem without journal. Opts: (null). Quota mode: none.
[ 9.816655] ext4 filesystem being mounted at /run/media/mmcblk2p11 supports timestamps until 2038 (0x7fffffff)
[ OK ] Mounted /run/media/mmcblk2p11.
[ OK ] Finished File System Check on /dev/mmcblk2p6.
Mounting /run/media/mmcblk2p6...
[ OK ] Finished File System Check on /dev/mmcblk2p5.
[ 10.084965] EXT4-fs (mmcblk2p6): mounted filesystem without journal. Opts: (null). Quota mode: none.
[ OK ] Mounted /run/media/mmcblk2p6.
Mounting /run/media/mmcblk2p5...
[ 10.155907] EXT4-fs (mmcblk2p5): mounted filesystem without journal. Opts: (null). Quota mode: none.
[ OK ] Mounted /run/media/mmcblk2p5.
[ OK ] Started User Manager for UID 0.
[ OK ] Started Session c1 of User root.
[ 10.551932] audit: type=1006 audit(1637342375.016:3): pid=811 uid=0 old-auid=4294967295 auid=0 tty=tty7 old-ses=4294967295 ses=2 res=1
[ 10.564126] audit: type=1300 audit(1637342375.016:3): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffc6b94ca0 a2=1 a3=ffff830cd6b0 items=0 ppid=1 pid=811 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=tty7 ses=2 comm="(weston)" exe="/lib/systemd/systemd" key=(null)
[ 10.590194] audit: type=1327 audit(1637342375.016:3): proctitle="(weston)"
[FAILED] Failed to start Weston, a …mpositor, as a system service.
See 'systemctl status weston.service' for details.
[ OK ] Reached target Graphical Interface.
Starting Record Runlevel Change in UTMP...
[ OK ] Finished Record Runlevel Change in UTMP.

NXP i.MX Release Distro 5.15-honister imx8mm-lpddr4-evk ttymxc1

imx8mm-lpddr4-evk login:

The BSP version is 5.15.5_1.0.0.

 

Does anyone got an idea?

Tags (4)
0 Kudos
Reply
1 Reply

1,192 Views
frk
Contributor III

Hi,

I've tried with the last release (Kirkstone imx-5.15.32-2.0.0) without success.

The display works well using HDMI but not with the OLED Screen.

0 Kudos
Reply