MMPF0100 can satisfy i.MX6SL power-down sequence?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MMPF0100 can satisfy i.MX6SL power-down sequence?

跳至解决方案
1,746 次查看
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6SL and MMPF0100.

Please see Table 14 in MCIMX6SLCEC Rev.3, it shows the power-down sequence.

I understand, if a i.MX6SL system cannot satify the power-down sequence, i.MX6SL is dameged in worst case, isn't it?

However, I did not find the power-down sequence of MMPF0100 in MMPF0100 datasheet.

Would you let me know whether MMPF0100 can satify the i.MX6SL power-down sequence?

Best Regards,

Satoshi Shimoda

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
1,448 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I.MX6SL will not be damaged using MMPF0100 and

such connection is recommended by IMX6SLHDG

Hardware Development Guide for i.MX 6SoloLite - User Guide

sect.3.2 Requirements for a generic interface between chip and PF0100.

However special power-down requirements may be applied if design uses E-INK

panels, they may require special power-down sequence and this is provided

by PMICs which are designed for such purposes (like TPS65185).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
8 回复数
1,449 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

I.MX6SL will not be damaged using MMPF0100 and

such connection is recommended by IMX6SLHDG

Hardware Development Guide for i.MX 6SoloLite - User Guide

sect.3.2 Requirements for a generic interface between chip and PF0100.

However special power-down requirements may be applied if design uses E-INK

panels, they may require special power-down sequence and this is provided

by PMICs which are designed for such purposes (like TPS65185).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
1,448 次查看
satoshishimoda
Senior Contributor I

Hi Igor,

As far as your reply, the conclusion is the following, right?

1. i.MX6SL has no special power-down sequence same as other i.MX6 chips when E-ink panel is NOT used.

2. The sequence in chapter 4.2.2 of MCIMX6SL (Rev.3) has to be applied when E-ink panel is used.

3. i.MX6SL will be not damaged by any power-down sequence when E-ink panel is not used, but damaged if the power-down sequence is not observed when E-ink panel is used.

Best Regards,

Satoshi Shimoda

0 项奖励
回复
1,448 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

1.2. right

3. i.MX6SL will be not damaged in that case too.

E-ink can.

Best regards

igor

1,448 次查看
satoshishimoda
Senior Contributor I

Hi Igor,

Umm, I'm confused why the power-down sequence is defined even though i.MX6SL will be not damaged in the both case E-ink is used or not.

Best Regards,

Satoshi Shimoda

0 项奖励
回复
1,448 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

connection is recommended by IMX6SLHDG

Hardware Development Guide for i.MX 6SoloLite - User Guide

and implemented on i.MX6SL EVK reference design.

Best regards

igor

0 项奖励
回复
1,448 次查看
satoshishimoda
Senior Contributor I

Hi Igor,

According to your reply, I understood i.MX6SL will be not damaged if use MMPF0100 and follow the Hardware Development Guide for i.MX6SoloLite, right?

Then, how about when user don't follow the recommended design?

Best Regards,

Satoshi Shimoda

0 项奖励
回复
1,448 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

in general connections in i.MX EVK reference designs are

considered as safe and recommended for usage - this is just

another option. For example AN3820 gives connection

MC34704B with i.MX25 which differs from datasheet, however

it can also be used as verified solution.

Best regards

igor

1,448 次查看
satoshishimoda
Senior Contributor I

Dear Igor,

Thank you for giving the another option.

I have one more question about power-down sequence, but this question is not related to MMPF0100.

So I will post a new question.

Thank you for your support.

Best Regards,

Satoshi Shimoda

0 项奖励
回复