Hi community,
I have a question about i.MX6SL and MMPF0100.
Please see Table 14 in MCIMX6SLCEC Rev.3, it shows the power-down sequence.
I understand, if a i.MX6SL system cannot satify the power-down sequence, i.MX6SL is dameged in worst case, isn't it?
However, I did not find the power-down sequence of MMPF0100 in MMPF0100 datasheet.
Would you let me know whether MMPF0100 can satify the i.MX6SL power-down sequence?
Best Regards,
Satoshi Shimoda
已解决! 转到解答。
Hi Satoshi
I.MX6SL will not be damaged using MMPF0100 and
such connection is recommended by IMX6SLHDG
Hardware Development Guide for i.MX 6SoloLite - User Guide
sect.3.2 Requirements for a generic interface between chip and PF0100.
However special power-down requirements may be applied if design uses E-INK
panels, they may require special power-down sequence and this is provided
by PMICs which are designed for such purposes (like TPS65185).
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Satoshi
I.MX6SL will not be damaged using MMPF0100 and
such connection is recommended by IMX6SLHDG
Hardware Development Guide for i.MX 6SoloLite - User Guide
sect.3.2 Requirements for a generic interface between chip and PF0100.
However special power-down requirements may be applied if design uses E-INK
panels, they may require special power-down sequence and this is provided
by PMICs which are designed for such purposes (like TPS65185).
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Igor,
As far as your reply, the conclusion is the following, right?
1. i.MX6SL has no special power-down sequence same as other i.MX6 chips when E-ink panel is NOT used.
2. The sequence in chapter 4.2.2 of MCIMX6SL (Rev.3) has to be applied when E-ink panel is used.
3. i.MX6SL will be not damaged by any power-down sequence when E-ink panel is not used, but damaged if the power-down sequence is not observed when E-ink panel is used.
Best Regards,
Satoshi Shimoda
Hi Igor,
According to your reply, I understood i.MX6SL will be not damaged if use MMPF0100 and follow the Hardware Development Guide for i.MX6SoloLite, right?
Then, how about when user don't follow the recommended design?
Best Regards,
Satoshi Shimoda
Hi Satoshi
in general connections in i.MX EVK reference designs are
considered as safe and recommended for usage - this is just
another option. For example AN3820 gives connection
MC34704B with i.MX25 which differs from datasheet, however
it can also be used as verified solution.
Best regards
igor
Dear Igor,
Thank you for giving the another option.
I have one more question about power-down sequence, but this question is not related to MMPF0100.
So I will post a new question.
Thank you for your support.
Best Regards,
Satoshi Shimoda