Dear community,
We consider the MMPF0100 register setting .
The SWxx_PWRSTG[2:0] bit control the number of power stage.
Meantime, SW1A/B/C has the parameter ( ISW1ABCLIM ) "Current Limiter Peak Current Detection"
Is the SWxx_PWRSTG[2:0] bit register setting related with the ISW1ABCLIM value ?
For example, the SWxx_PWRSTG[2:0] is set to "001" (about half power),
then Does ISW1ABCLIM value decrease ?
Best Regards,
Koichi Sakagami
已解决! 转到解答。
Hi koichi
no ISW1ABCLIM does not decrease (SWxx_PWRSTG[2:0] setting not related with the ISW1ABCLIM value),
it has fixed value described in Table 53 SW1A/B/C Electrical Characteristics MMPF0100
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi koichi
no ISW1ABCLIM does not decrease (SWxx_PWRSTG[2:0] setting not related with the ISW1ABCLIM value),
it has fixed value described in Table 53 SW1A/B/C Electrical Characteristics MMPF0100
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------