MMPF0100 : Is the the SWxx_PWRSTG[2:0] setting related with the ISW1ABCLIM value ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMPF0100 : Is the the SWxx_PWRSTG[2:0] setting related with the ISW1ABCLIM value ?

Jump to solution
605 Views
koichisakagami
Contributor II

Dear community,

We consider the MMPF0100 register setting .

The SWxx_PWRSTG[2:0] bit control the number of power stage.
Meantime, SW1A/B/C has the parameter ( ISW1ABCLIM ) "Current Limiter Peak Current Detection"

Is the SWxx_PWRSTG[2:0] bit register setting related with the ISW1ABCLIM value ?
For example, the SWxx_PWRSTG[2:0] is set to "001" (about half power),
then Does ISW1ABCLIM value decrease ?

Best Regards,
Koichi Sakagami

Labels (1)
0 Kudos
Reply
1 Solution
525 Views
igorpadykov
NXP Employee
NXP Employee

Hi koichi

no ISW1ABCLIM does not decrease (SWxx_PWRSTG[2:0] setting not related with the ISW1ABCLIM value),

it has fixed value described in Table 53 SW1A/B/C Electrical Characteristics MMPF0100

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
526 Views
igorpadykov
NXP Employee
NXP Employee

Hi koichi

no ISW1ABCLIM does not decrease (SWxx_PWRSTG[2:0] setting not related with the ISW1ABCLIM value),

it has fixed value described in Table 53 SW1A/B/C Electrical Characteristics MMPF0100

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply