I'm using a custom board which sports an iMX6 SOLO running Yocto with Kernel version 4.9.11-02307-gb200f6d.
My application uses serial communication with RS485 transceiver attached to the serial comms.
Pin control configuration -DTS- and UART initialization are described below.
There is no problem with such configuration when frame length sent through the serial ports is below 20-30 bytes but when frame length is above these values, eventually -sometimes it takes some minutes- the whole system hangs -by 'hangs' I meant that system gets unresponsive and I can't even connect through SSH, needing to restart Linux-
A simple while(1) sending a single byte causes this problem within seconds.
The problem is not related to one specific UART as it happens on other 3 UARTs configured the same way.
If I insert a delay when sending those bytes the problem never happens but obviously, this is not a satisfactory solution.
Is there something that I'm missing that could cause this issue?
DTS configuration:
&uart2 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_uart2_3>;
fsl,uart-has-rtscts;
status = "okay";
};
pinctrl_uart2_3: uart2grp-3 {
fsl,pins = <
MX6QDL_PAD_EIM_D27__UART2_RX_DATA 0x1b0b1
MX6QDL_PAD_EIM_D26__UART2_TX_DATA 0x1b0b1
MX6QDL_PAD_EIM_D28__UART2_CTS_B 0x1b0b1
>;
};
UART inicialization:
int rs485 = ::open("/dev/ttymxc1");
if(rs485) {
struct serial_rs485 rs485conf;
rs485conf.flags = 0x00;
rs485conf.flags |= SER_RS485_ENABLED;
rs485conf.flags |= SER_RS485_RTS_ON_SEND;
if (ioctl (rs485, TIOCSRS485, &rs485conf) < 0) {
qDebug() << QString("Error writing ioctl port (%1): %2").arg(errno).arg(strerror(errno));
return false;
}
}
UART stress -running in a separate thread-:
char byte = 0xff;
while(1) {
writeData(&byte, 1);
}
Thanks in advance.
已解决! 转到解答。
Hi Miguel
one can try with nxp releases from linux-imx - i.MX Linux kernel
or better with latest linux L4.14.78
Also one can try to disable uart sdma and use polling option.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Miguel
one can try with nxp releases from linux-imx - i.MX Linux kernel
or better with latest linux L4.14.78
Also one can try to disable uart sdma and use polling option.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thks Igor.
I followed your last suggestion and disabled DMA for both Tx/Rx in DTS files.
uart2: serial@021e8000 {
compatible = "fsl,imx6q-uart", "fsl,imx21-uart";
reg = <0x021e8000 0x4000>;
interrupts = <0 27 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&clks IMX6QDL_CLK_UART_IPG>,
<&clks IMX6QDL_CLK_UART_SERIAL>;
clock-names = "ipg", "per";
/*dmas = <&sdma 27 4 0>, <&sdma 28 4 0>;
dma-names = "rx", "tx";*/
status = "disabled";
};
This way solves the issue and now the system never hangs. Also this change increases the UART performance for short frames length -we usually transmit blocks with less than 32 bytes which is below the Tx FIFO length-.
I'll dig into this problem to find out why UART's DMA could cause such behavior.
Regards