LVDS1 DISPLAY ON SABRE-SDP IMX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LVDS1 DISPLAY ON SABRE-SDP IMX6DL

593 Views
kapilkumar
Contributor III

Hi

is it possible to get live video streaming on the single LVDS display  through two camera..? camera 1 is suppose parallel camera and other is serial camera.

Thanks & Regards,

Kapil Kumar.

Labels (3)
0 Kudos
Reply
1 Reply

504 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please refer to section 7.3.1.6.3 (Multiple videos overlay) of "i.MX_Linux_User's_Guide.pdf"

of the recent NXP BSP (please use it) :

< https://www.nxp.com/webapp/Download?colCode=L3.14.52_1.1.0_MX6QDLSOLO&appType=license&location=null >

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply