Hello,
Started to build the source packages for IMx6Q baord. The release is L3.0.15_12.04.01_ER_source and end up getting buil dissues with LTLIB.
Here is the log of the error.
*************************************
Processing: mtd-utils
=======================
Build path taken because: no prebuilt rpm,
Testing network connectivity
OK GPP:
Try mtd-utils-201006.tar.bz2.md5 from the GPP
http://bitshrine.org/gpp/mtd-utils-201006.tar.bz2.md5:
11:52:39 ERROR 404: Not Found.
Try mtd-utils-201006.tar.bz2 from the GPP
http://bitshrine.org/gpp/mtd-utils-201006.tar.bz2:
11:52:39 ERROR 404: Not Found.
Can't get: mtd-utils-201006.tar.bz2 at ./ltib line 790.
Died at ./ltib line 1380.
traceback:
main::build_host_rpms:1380
main::host_checks:1435
main:542
Started: Mon Oct 1 11:52:36 2012
Ended: Mon Oct 1 11:52:39 2012
Elapsed: 3 seconds
These packages failed to build:
mtd-utils
Build Failed
**************************************************
How can this be sorted out. My environment is a Ubuntu 10.04 lucid.
Any inputs will be highly appreciated.
Thanks,
mep
Solved! Go to Solution.
I meet the same problem but under linux version 3.2.0. I find inside the ltib/dist/lfs-5.1/mtd-utils folder a other file .spec (mtd-utils-20060302.spec) which worked on my plateform
I'm getting the same on L3.0.35_12.09.01. I applied mtd-utils-201006-4K-218-224-support.patch, and still could not build. I tried to apply mtd-utils-201006-remove-Werror-for-old-utils.patch, but it breaks. The mfgtool2 image does not include kernel headers, and I need kernel headers to build my code, hence I NEED to build this kernel. Somehow Freescale was able to build the kernel. PLEASE could that person let us know how to get around this error? Web searches have not provided a solution, and ltib tries to get mtd-utils-201006 from a site that no longer provides this older version of mtd-utils.
jc3@jc3-ubuntu:~/.local/share/Trash/files/mtd-utils$ make
gcc -I./include -D_FILE_OFFSET_BITS=64 -O2 -g -Wall -Wextra -Wwrite-strings -Wno-sign-compare -c -o /home/jc3/.local/share/Trash/files/mtd-utils/nanddump.o nanddump.c -g -Wp,-MD,/home/jc3/.local/share/Trash/files/mtd-utils/.nanddump.c.dep
nanddump.c: In function ‘main’:
nanddump.c:347: warning: ignoring return value of ‘write’, declared with attribute warn_unused_result
nanddump.c:350: warning: ignoring return value of ‘write’, declared with attribute warn_unused_result
nanddump.c:376: warning: ignoring return value of ‘write’, declared with attribute warn_unused_result
nanddump.c:389: warning: ignoring return value of ‘write’, declared with attribute warn_unused_result
nanddump.c:392: warning: ignoring return value of ‘write’, declared with attribute warn_unused_result
gcc -O2 -g -Wall -Wextra -Wwrite-strings -Wno-sign-compare -g -o /home/jc3/.local/share/Trash/files/mtd-utils/nanddump /home/jc3/.local/share/Trash/files/mtd-utils/nanddump.o
gcc -I./include -D_FILE_OFFSET_BITS=64 -O2 -g -Wall -Wextra -Wwrite-strings -Wno-sign-compare -c -o /home/jc3/.local/share/Trash/files/mtd-utils/mkfs.jffs2.o mkfs.jffs2.c -g -Wp,-MD,/home/jc3/.local/share/Trash/files/mtd-utils/.mkfs.jffs2.c.dep
mkfs.jffs2.c:69:21: error: sys/acl.h: No such file or directory
mkfs.jffs2.c: In function ‘recursive_add_host_directory’:
mkfs.jffs2.c:435: warning: ignoring return value of ‘asprintf’, declared with attribute warn_unused_result
mkfs.jffs2.c:440: warning: ignoring return value of ‘asprintf’, declared with attribute warn_unused_result
mkfs.jffs2.c:442: warning: ignoring return value of ‘asprintf’, declared with attribute warn_unused_result
mkfs.jffs2.c: In function ‘interpret_table_entry’:
mkfs.jffs2.c:533: warning: ignoring return value of ‘asprintf’, declared with attribute warn_unused_result
mkfs.jffs2.c:600: warning: ignoring return value of ‘asprintf’, declared with attribute warn_unused_result
mkfs.jffs2.c:601: warning: ignoring return value of ‘asprintf’, declared with attribute warn_unused_result
mkfs.jffs2.c: At top level:
mkfs.jffs2.c:1095: warning: initialization discards qualifiers from pointer target type
mkfs.jffs2.c:1096: warning: initialization discards qualifiers from pointer target type
mkfs.jffs2.c:1097: warning: initialization discards qualifiers from pointer target type
mkfs.jffs2.c:1098: warning: initialization discards qualifiers from pointer target type
mkfs.jffs2.c:1099: warning: initialization discards qualifiers from pointer target type
mkfs.jffs2.c: In function ‘formalize_posix_acl’:
mkfs.jffs2.c:1123: error: ‘ACL_USER_OBJ’ undeclared (first use in this function)
mkfs.jffs2.c:1123: error: (Each undeclared identifier is reported only once
mkfs.jffs2.c:1123: error: for each function it appears in.)
mkfs.jffs2.c:1124: error: ‘ACL_GROUP_OBJ’ undeclared (first use in this function)
mkfs.jffs2.c:1125: error: ‘ACL_MASK’ undeclared (first use in this function)
mkfs.jffs2.c:1126: error: ‘ACL_OTHER’ undeclared (first use in this function)
mkfs.jffs2.c:1132: error: ‘ACL_USER’ undeclared (first use in this function)
mkfs.jffs2.c:1133: error: ‘ACL_GROUP’ undeclared (first use in this function)
mkfs.jffs2.c: In function ‘recursive_populate_directory’:
mkfs.jffs2.c:1336: warning: format ‘%9lu’ expects type ‘long unsigned int’, but argument 3 has type ‘__off64_t’
mkfs.jffs2.c:1345: warning: format ‘%9lu’ expects type ‘long unsigned int’, but argument 3 has type ‘__off64_t’
mkfs.jffs2.c:1354: warning: format ‘%9lu’ expects type ‘long unsigned int’, but argument 3 has type ‘__off64_t’
mkfs.jffs2.c:1384: warning: format ‘%9lu’ expects type ‘long unsigned int’, but argument 3 has type ‘__off64_t’
mkfs.jffs2.c:1395: warning: format ‘%9lu’ expects type ‘long unsigned int’, but argument 3 has type ‘__off64_t’
mkfs.jffs2.c: At top level:
mkfs.jffs2.c:1519: warning: initialization discards qualifiers from pointer target type
mkfs.jffs2.c:1521: warning: initialization discards qualifiers from pointer target type
mkfs.jffs2.c: In function ‘main’:
mkfs.jffs2.c:1881: warning: passing argument 2 of ‘recursive_add_host_directory’ discards qualifiers from pointer target type
mkfs.jffs2.c:403: note: expected ‘char *’ but argument is of type ‘const char *’
make: *** [/home/jc3/.local/share/Trash/files/mtd-utils/mkfs.jffs2.o] Error 1
rm /home/jc3/.local/share/Trash/files/mtd-utils/nanddump.o
I am also getting this error.
Stephane for newbies can you list the steps to use the .spec file?
Please find enclosed a link to
Thanks for your reply and help! Yesterday I was able to get the entire kernel and root file system for all supported programs working under Ubuntu 12.04. Now I can work on MY application...