I had a problem running LTIB. All the host packages are installed.
i could see the list of packages required for LTIB in /opt/freescale/pkgs.
user@ubuntu:/mnt/hgfs/Shared/IMX/L2.6.35_10.12.01_ER_source/home/ltib$ ./ltib
Installing host support packages.
This only needs to be done once per host, but may take up to
an hour to complete ...
If an error occurs, a log file with the full output may be found in:
/mnt/hgfs/Shared/IMX/L2.6.35_10.12.01_ER_source/home/ltib/host_config.log
Exiting on error or interrupt
Please see >> /mnt/hgfs/Shared/IMX/L2.6.35_10.12.01_ER_source/home/ltib/host_config.log for details
i have attached the host_config_1.log
i dont understand if it is a problem witht .gvfs permission denial
or with the mkspooflinks package(mkspooflinks is present in /opt/freescale/pkgs)
finnaly build is failing.
I dont know what's going wrong here and hope that somebody can help me.
Hi Gopi Sriram,
From you config_log
Cowardly refusing to clobber existing directory:
/opt/freescale/ltib/usr/src/rpm/BUILD/mkspooflinks-3.4
Remove this by hand if you really want to rebuild this package from scratch
Remove that directory, and build again.
Also, if you are using 11.09 BSP or later / if you are using Ubuntu-11.04, then there are certain patches needed.
I don't think that was an issue with your build.
But check that also.
.gvfs warnings are quite normal.No need to worry about them more.
Regards :: Krishna Pavan
i ran with the option ./ltib -v
attached the host_config.log for this option
Thanks Krishna for the reply
these all files are there in the /opt/freescale/pkgs
mkspooflinks-3.4-ccache.patch
mkspooflinks-3.4-ccache.patch.md5
mkspooflinks-3.4-filter-link-paths.patch
mkspooflinks-3.4-filter-link-paths.patch.md5
mkspooflinks-3.4-mmlink.patch
mkspooflinks-3.4-mmlink.patch.md5
mkspooflinks-3.4-prefixbefore.patch
mkspooflinks-3.4-prefixbefore.patch.md5
mkspooflinks-3.4.tar.gz
mkspooflinks-3.4.tar.gz.md5
are these insufficient
Thanks
Gopi
Hi,
Check if mkspooflinks developer files are available on your host?
Regards :: Krishna Pavan