Hi,
I am trying to install LTIB from L2.6.35_11.09.01_ER_source_bundle.tar.gz for i.mx53 under Ubunto 14.04 64 bit.
the build fails and I get the following error:
--------------------------
checking whether the C compiler (/home/haim/Downloads/gcc-linaro-5.2-2015.11-x86_64_arm-linux-gnueabihf/bin/arm-linux-gnueabihf- ) works... no
configure: error: installation or configuration problem: C compiler cannot create executables.
error: Bad exit status from /home/haim/imx53-sw/ltib/tmp/rpm-tmp.UZAHzv (%build)
RPM build errors:
Bad exit status from /home/haim/imx53-sw/ltib/tmp/rpm-tmp.UZAHzv (%build)
Build time for rpm-fs: 2 seconds
Failed building rpm-fs
could not glob rpm in: /tmp/rpm-haim/RPMS/x86_64/rpm-fs-* at ./ltib line 2410.
traceback:
main::check_rpm_setup:2410
main::host_checks:1423
main:542
Started: Sun Jan 3 12:12:21 2016
Ended: Sun Jan 3 12:12:24 2016
Elapsed: 3 seconds
These packages failed to build:
rpm-fs
Build Failed
---------------------
any thoughts?
Hello,
Please check if environment setup is correct, as recommended
for LTIB. Please refer to the enclosed.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
thanks for your reply,
the pdf you enclosed was written for ubuntu 9.04.
Is is still valid to ubuntu 14.04? are there any patches needed?