Hi All,
I was wondering how to choose between these 2 modes in a design using the PF0100 PMIC.
Indeed i don't see what are the benefits to run in LDO-bypass except to reduce power dissipation inside the iMX6.
On the other hand i read in the AN4724 : Longer power-on-hours can be achieved using LDO-enabled mode
Please help me to understand.
Greg
HI gregory
for description please look at sect.4.1.2 Linux kernel image and device tree
attached Linux Guide from L3.14.28_1.0.0_iMX6QDLS_BUNDLE
Purpose of ldo bypas is to reduce overal power consumption and heating
of processor, this is very important in portable applications.
In ldo bypas one needs to control PMIC for using Dynamic Bus Frequency and
CPU Frequency Scaling (CPUFREQ) Driver. This is described in Linux
Manual Chapter 24,25.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------