Hi Everyone,
We are planning to use "BD070LIC1 – 7″ 1280×800 Display" with Touchscreen for our project.
The connectors in the LCD + Touchscreen is not compatible with our host board, So we have decided to use a intermediate connector board.
Details of the host board :
Please find attached schematics, Can anyone please make sure the LCD will work with Sabre SDP. Also recommend if any other 7" LVDS LCD is compatible for our host board.
Ref:
Host board - SABRE for Smart Devices Reference Design|Freescale
Original present Working LCD - http://boundarydevices.com/wp-content/uploads/2013/06/HSD100PXN1-A00-C11-1.0.pdf
The LCD we are going to use - http://boundarydevices.com/wp-content/uploads/2014/12/HSD070PWW1-B01.pdf
The Touchscreen we are going to use - http://boundarydevices.com/wp-content/uploads/2015/05/SE-CTPGG7007.pdf#page=1&zoom=170,402,836
Regards,
Venkat
已解决! 转到解答。
The solution you consider seems to be the working one. You then have to adjust the screen resolution parameters in display driver and correctly handle the touchscreen by I2C interface.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
The solution you consider seems to be the working one. You then have to adjust the screen resolution parameters in display driver and correctly handle the touchscreen by I2C interface.
Have a great day,
Artur
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------