LAN8720 and IMX287

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LAN8720 and IMX287

971 Views
royho
Contributor I

​Dear community,

we are experiencing something as follow:

tthe system is trying to get the IP address from the router through dhcp during bootup

we got the following:

Sending discover...

PHY: 0:00 - Link is Up - 100/Full

Sending discover...

PHY: 0:00 - Link is Down

Sending discover...

PHY: 0:00 - Link is Up - 100/Full

Resetting PHY

No lease, failing

after that, we asked to eth0 to up and get IP, it works perfectly ( we can ping like 1 hr without any problem)

it just couldn't get the IP when bootup

In 50 pcs of our prototype, around 15pcs couldn't get the IP at bootup

Anyone can point me to some direction where to look at?

thanks

roy

Labels (2)
0 Kudos
Reply
2 Replies

726 Views
igorpadykov
NXP Employee
NXP Employee

Hi Roy

recommended to use latest FSL BSP on link below with all patches on bottom that page,

one can try attached patch

L2.6.35 10.12 FEC0 PATCH (REV 2010.12.01)

Linux patch for i.MX28 SDK 2010.12 to fix the ethernet FEC0 conection problem on i.MX28 EVK

i.MX28 Evaluation Kit|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

726 Views
royho
Contributor I

Hi igor,

Will try

Thanks

Roy

0 Kudos
Reply