Kernel Panic in GPU driver on i.mx 53 (Internal error Oops: 817 )

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Kernel Panic in GPU driver on i.mx 53 (Internal error Oops: 817 )

960 次查看
alexeinomazov
Contributor II

Hello,

I experience kernel panic when executing simple Qt application with gif animation or images presentation.

From kernel logs it seems to be known situation within GPU driver code specific location:

"kernel BUG at drivers/mxc/amd-gpu/platform/hal/linux/misc.c:66! "

Platform:

i.mx 53 board with linux kernel 2.6.35.

Yocto layer with Qt 5.4.1 over Linux X11.

Kernel Log:

kernel BUG at drivers/mxc/amd-gpu/platform/hal/linux/misc.c:66!

Unable to handle kernel NULL pointer dereference at virtual address 00000000

pgd = 80004000

[00000000] *pgd=00000000

Internal error: Oops: 817 [#1] PREEMPT

last sysfs file: /sys/module/fec/parameters/g_phy_addr

Modules linked in: pl2303 cp210x

CPU: 0    Not tainted  (2.6.35.3-744-g27fdf7b #9)

PC is at __bug+0x18/0x24

LR is at __bug+0x14/0x24

pc : [<80095ddc>]    lr : [<80095dd8>]    psr: 200f0193

sp : 80925f10  ip : 968fc000  fp : 00000000

r10: 0000001f  r9 : 80924000  r8 : 00000001

r7 : 00000001  r6 : a00f0193  r5 : 00000000  r4 : 9552f240

r3 : 00000000  r2 : 80925f04  r1 : 8087c1d1  r0 : 00000046

Flags: nzCv  IRQs off  FIQs on  Mode SVC_32  ISA ARM  Segment kernel

Control: 10c5387d  Table: 858e4019  DAC: 00000017

Process swapper (pid: 0, stack limit = 0x809242e8)

Stack: (0x80925f10 to 0x80926000)

5f00:                                     9552f240 803ffde8 809a0f98 00000000

5f20: 00000000 0000000c 00000001 803f9978 9507df00 803feea8 9507df00 800edc94

5f40: 809441e4 0000000c 9507df00 00000002 00000001 800efd5c 0000000c 00000000

5f60: 00000001 8009206c ffffffff 96800000 00000001 80092a8c 809329ec 03c5dc3c

5f80: 00000001 00000000 80924000 80928a30 8097b3a4 80928a28 7002bca0 412fc085

5fa0: 0000001f 00000000 00000003 80925fc0 80093a84 80093a88 600f0013 ffffffff

5fc0: 80924000 80093f6c 80986da0 80928ad0 8002d5c4 80008994 800084e8 00000cc9

5fe0: 70000100 8002d5c4 10c53c7d 8097b450 8002d5c0 70008034 00000000 00000000

[<80095ddc>] (__bug+0x18/0x24) from [<803ffde8>] (_kgsl_device_active+0x78/0x158)

[<803ffde8>] (_kgsl_device_active+0x78/0x158) from [<803f9978>] (kgsl_intr_isr+0x44/0x60)

[<803f9978>] (kgsl_intr_isr+0x44/0x60) from [<803feea8>] (z430_irq_handler+0x8/0x10)

[<803feea8>] (z430_irq_handler+0x8/0x10) from [<800edc94>] (handle_IRQ_event+0x24/0xe4)

[<800edc94>] (handle_IRQ_event+0x24/0xe4) from [<800efd5c>] (handle_level_irq+0xd4/0x180)

[<800efd5c>] (handle_level_irq+0xd4/0x180) from [<8009206c>] (asm_do_IRQ+0x6c/0x8c)

[<8009206c>] (asm_do_IRQ+0x6c/0x8c) from [<80092a8c>] (__irq_svc+0x4c/0xcc)

Exception stack(0x80925f78 to 0x80925fc0)

5f60:                                                       809329ec 03c5dc3c

5f80: 00000001 00000000 80924000 80928a30 8097b3a4 80928a28 7002bca0 412fc085

5fa0: 0000001f 00000000 00000003 80925fc0 80093a84 80093a88 600f0013 ffffffff

[<80092a8c>] (__irq_svc+0x4c/0xcc) from [<80093a88>] (default_idle+0x24/0x28)

[<80093a88>] (default_idle+0x24/0x28) from [<80093f6c>] (cpu_idle+0x48/0xa0)

[<80093f6c>] (cpu_idle+0x48/0xa0) from [<80008994>] (start_kernel+0x270/0x2c4)

[<80008994>] (start_kernel+0x270/0x2c4) from [<70008034>] (0x70008034)

Code: e92d4010 e59f000c eb11eae6 e3a03000 (e5833000)

---[ end trace d941ea1388c9cbad ]---

Kernel panic - not syncing: Fatal exception in interrupt

[<800974ac>] (unwind_backtrace+0x0/0xf0) from [<805108dc>] (panic+0x6c/0x104)

[<805108dc>] (panic+0x6c/0x104) from [<80096388>] (die+0x2b4/0x304)

[<80096388>] (die+0x2b4/0x304) from [<800982e0>] (__do_kernel_fault+0x64/0x84)

[<800982e0>] (__do_kernel_fault+0x64/0x84) from [<800984c0>] (do_page_fault+0x1c0/0x1d4)

[<800984c0>] (do_page_fault+0x1c0/0x1d4) from [<800922b8>] (do_DataAbort+0x34/0x94)

[<800922b8>] (do_DataAbort+0x34/0x94) from [<80092a2c>] (__dabt_svc+0x4c/0x60)

Exception stack(0x80925ec8 to 0x80925f10)

5ec0:                   00000046 8087c1d1 80925f04 00000000 9552f240 00000000

5ee0: a00f0193 00000001 00000001 80924000 0000001f 00000000 968fc000 80925f10

5f00: 80095dd8 80095ddc 200f0193 ffffffff

[<80092a2c>] (__dabt_svc+0x4c/0x60) from [<80095ddc>] (__bug+0x18/0x24)

[<80095ddc>] (__bug+0x18/0x24) from [<803ffde8>] (_kgsl_device_active+0x78/0x158)

[<803ffde8>] (_kgsl_device_active+0x78/0x158) from [<803f9978>] (kgsl_intr_isr+0x44/0x60)

[<803f9978>] (kgsl_intr_isr+0x44/0x60) from [<803feea8>] (z430_irq_handler+0x8/0x10)

[<803feea8>] (z430_irq_handler+0x8/0x10) from [<800edc94>] (handle_IRQ_event+0x24/0xe4)

[<800edc94>] (handle_IRQ_event+0x24/0xe4) from [<800efd5c>] (handle_level_irq+0xd4/0x180)

[<800efd5c>] (handle_level_irq+0xd4/0x180) from [<8009206c>] (asm_do_IRQ+0x6c/0x8c)

[<8009206c>] (asm_do_IRQ+0x6c/0x8c) from [<80092a8c>] (__irq_svc+0x4c/0xcc)

Exception stack(0x80925f78 to 0x80925fc0)

5f60:                                                       809329ec 03c5dc3c

5f80: 00000001 00000000 80924000 80928a30 8097b3a4 80928a28 7002bca0 412fc085

5fa0: 0000001f 00000000 00000003 80925fc0 80093a84 80093a88 600f0013 ffffffff

[<80092a8c>] (__irq_svc+0x4c/0xcc) from [<80093a88>] (default_idle+0x24/0x28)

[<80093a88>] (default_idle+0x24/0x28) from [<80093f6c>] (cpu_idle+0x48/0xa0)

[<80093f6c>] (cpu_idle+0x48/0xa0) from [<80008994>] (start_kernel+0x270/0x2c4)

[<80008994>] (start_kernel+0x270/0x2c4) from [<70008034>] (0x70008034)

Questions:

1). Which scenarios related to the known issue "kernel BUG at drivers/mxc/amd-gpu/platform/hal/linux/misc.c:66! " ?

2). Which scenario could be related to my application (Qt based gif / image presentation) ?

3). How can i potentially avoid it ?

Any help would be appreciated.

Thanks,

Alexei.

0 项奖励
回复
1 回复

642 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Alexei

for Qt building one can refer to

Building Qt for i.MX5x

regarding this error suggest to post on meta-fsl-arm mailing list,

so more people could try to assist you

https://lists.yoctoproject.org/listinfo/meta-freescale

Best regards

igor

0 项奖励
回复